Last updated: 2010-03-10
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the MS RX Frequency Step Values. You can set up to 40 values as the MS Rx Frequency step. Which Frequency step levels are to be actually used for the measurement are also defined by Frequency Start Index and Number of Frequency Step. The test set allows you to set the frequency across different bands (see Channel). |
|
Setting |
Range: 1880.0 to 1920.0, 2010.0 to 2025.0 MHz Resolution: 0.01 Hz |
|
Query |
Same as setting |
|
*RST Setting |
1880.8, 1900.0, 1919.2, 2010.8, 2024.2, [2023.8 to 011.0 (step= -1.6)], [1919.2 to 1880.0 (step = -1.6)], 2017.4 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:FREQuency:STEP 1880.8, 1900.0, 1919.2, 2010.8, 2024.2, 2017.4" |
|
Function |
Sets/queries the Number of Rx Frequency Steps. |
|
Setting |
Range: 1 to 40 Resolution: 1 |
|
Query |
Range: 1 to 40 |
|
*RST Setting |
5 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:FREQuency:STEP:COUNt 5" |
|
Function |
Sets/queries the Rx Frequency Start Index. |
|
Setting |
Range: 0 to 39 Resolution: 1 |
|
Query |
Range: 0 to 39 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:FREQuency:STEP:STARt 0" |
|
Function |
Sets/queries the MS RX Power Step Levels. You can set up to 40 values as the MS Rx Power step. Which power step levels are to be actually used for the measurement are also defined by MS RX Power Start Index and Number of MS RX Power Step. |
|
Setting |
Range: +37 to -165. Resolution: 0.01 |
|
Query |
Range: +37 to -165 |
|
*RST Setting |
-105.0, -95.0, -85.0, -75.0, -65.0, -55.0, -45.0, -35.0, -25.0, -15.0, -20.0, -30.0, -40.0, -50.0, -60.0, -70.0, -80.0, -90.0, -100.0 , -97.5, -92.5, -87.5, -82.5, -77.5, -72.5, -67.5, -62.5, -57.5, -52.5, -47.5, -42.5, -37.5, -32.5, -27.5, -22.5, -17.5, -19.0, -29.0, -39.0, -49.0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:POWer:STEP -105.0, -95.0, -85.0, -75.0, -65.0, -55.0, -45.0, -35.0, -25.0, -15.0, -20.0, -30.0, -40.0, -50.0, -60.0, -70.0, -80.0, -90.0, -100.0 , -97.5, -92.5, -87.5, -82.5, -77.5, -72.5, -67.5, -62.5, -57.5, -52.5, -47.5, -42.5, -37.5, -32.5, -27.5, -22.5, -17.5, -19.0, -29.0, -39.0, -49.0" |
|
Function |
Sets/queries the Number of MS Rx Power Steps . |
|
Setting |
Range: 1 to 40 Resolution: 1 |
|
Query |
Same as setting |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:POWer:STEP:COUNt 10" |
|
Function |
Sets/queries the Rx Power Step Length. The unit is Subframe (5ms). |
|
Setting |
Range: 1 to 10 Resolution: 1 |
|
Query |
Range: 1 to 10 |
|
*RST Setting |
1 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:POWer:STEP:LENGth 1" |
|
Function |
Sets/queries the MS RX Frequency Step Start Index . |
|
Setting |
Range: 0 to 39 Resolution: 1 |
|
Query |
Range: 0 to 39 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:RX:POWer:STEP:STARt 0" |
|
Function |
Sets/queries the MS Tx Frequency Step Values. You can set up to 40 values as the MS Tx Frequency step. Which Frequency step levels are to be actually used for the measurement are also defined by Tx Frequency Start Index and Number of MS Tx Frequency Step. The test set allows you to set the frequency across different bands (see Channel). |
|
Setting |
Range: 1880.0 to 1920.0, 2010.0 to 2025.0 |
|
Query |
Range: 1880.0 to 1920.0, 2010.0 to 2025.0 |
|
*RST Setting |
1880.8,1900.0,1919.2,2010.8,2024.2,[2023.8 to 2011.0 (step = -1.6], [1919.2 to 1880.0 (step = -1.6)], 2017.4 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:FREQuency:STEP 1880.8,1900.0,1919.2,2010.8,2024.2, 2017.4" |
|
Function |
Sets/queries the Number of Tx Frequency Steps. |
|
Setting |
Range: 1 to 40 Resolution: 1 |
|
Query |
Range: 1 to 40 |
|
*RST Setting |
5 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:FREQuency:STEP:COUNt 5" |
|
Function |
Sets/queries the Tx Frequency Start Index. |
|
Setting |
Range: 0 to 39 Resolution: 1 |
|
Query |
Range: 0 to 39 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:FREQuency:STEP:STARt 0" |
|
Function |
Sets/queries the MS TX Power Step Levels. You can set up to 40 values as the MS Tx Power step. Which power step levels are to be actually used for the measurement are also defined by Tx Power Start Index and Number of Tx Power Step. |
|
Setting |
Range: +80 to -120 Resolution: 0.01 |
|
Query |
Range: +80 to -120 |
|
*RST Setting |
+24.0, +21.0, +15.0, +5.0, -5.0, -15.0, -25.0, -35.0, -45.0, -55.0, -50.0, -40.0, -30.0, -20.0, -10.0, -0.0, +10.0, +20.0, +17.5, +12.5, +7.5, +2.5, -2.5, -7.5, -12.5, -17.5, -22.5, -27.5, -32.5, -37.5, -42.5, -47.5, -52.5, -49.0, -39.0, -29.0, -19.0, -9.0, 1.0, 11.0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:POWer:STEP +24.0, +21.0, +15.0, +5.0, -5.0, -15.0, -25.0, -35.0, -45.0, -55.0, -50.0, -40.0, -30.0, -20.0, -10.0, -0.0, +10.0, +20.0, +17.5, +12.5, +7.5, +2.5, -2.5, -7.5, -12.5, -17.5, -22.5, -27.5, -32.5, -37.5, -42.5, -47.5, -52.5, -49.0, -39.0, -29.0, -19.0, -9.0, 1.0, 11.0" |
|
Function |
Sets/queries the Number of Tx Power Steps . |
|
Setting |
Range: 1 to 40 Resolution: 1 |
|
Query |
Same as setting |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:POWer:STEP:COUNt 10" |
|
Function |
Sets/queries the MS TX Frequency Step Start Index . |
|
Setting |
Range: 0 to 39 Resolution: 1 |
|
Query |
Range: 0 to 39 Resolution: 1 |
|
*RST Setting |
0 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:MS:TX:POWer:STEP:STARt 1" |
|
Function |
The setting form of this command performs two functions: (1) sets the Fast Device Tune measurement's timeout (see Measurement Timeouts ) value, and (2) sets the Fast Device Tune measurement's timeout state to 1 (on). The query form returns the Fast Device Tune measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 seconds, off |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:TIMeout 5s" |
|
Function |
Sets/queries Fast Device Tune measurement's timeout state (see Measurement Timeout). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:TIMeout:STATe ON" |
|
Function |
Sets/queries Fast Device Tune measurement's timeout (see Measurement Timeout) setting to be used when the timeout state is set to ON. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 seconds |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TFDTune:TIMeout:TIME 5S" |