Last updated: 2010-03-10
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the BLER criteria for transmitted at Median_CQI. If the calculated BLER rate for median CQI is higher than this setting, Report of CQI measurement will fail the UE. |
|
Setting |
Range: 0 to 100 % Resolution: 0.01 |
|
Query |
Same as setting |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:BLERatio:TRANsmit:MCQI 10" |
|
Function |
Sets/queries the Number of CQI Reports to test. |
|
Setting |
Range: 1 to 99000 Resolution: 1 |
|
Query |
Same as setting |
|
*RST Setting |
2000 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:CQIReports 2000" |
|
Function |
Sets/queries the Percentage of CQI values within range. |
|
Setting |
Range: 0 to 100 % |
|
Query |
Same as setting |
|
*RST Setting |
90 (%) |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:CQIValues:WRANge 90" |
|
Function |
Sets/queries the Permitted CQI range from median |
|
Setting |
Range: 0 to 5 Resolution: 1 |
|
Query |
Same as setting |
|
*RST Setting |
2 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:RANGe:FMEDian 2" |
|
Function |
The setting form of this command performs two functions: (1) sets the measurement's timeout value (see Measurement Timeout), and (2) sets the measurement's timeout state to 1 (on). The query form returns the measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Same as setting |
|
*RST Setting |
Timeout value: 20 seconds Timeout state: off |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:TIMeout 20" |
|
Function |
Sets/queries the measurement's timeout state (see Measurement Timeout). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:TIMeout:STATe 0" |
|
Function |
Sets/queries the measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeout). |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Same as setting |
|
*RST Setting |
20 seconds |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:TIMeout:TIME 20" |
|
Function |
Sets/queries the Number transmitted at Median CQI to test. |
|
Setting |
Range: 1 to 99000 Resolution: 1 |
|
Query |
Same as setting |
|
*RST Setting |
1000 |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:THCQuality:TRANsmit:MCQI 1000" |