SETup:TOOPower

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions.

For the measurement, see Transmit ON/OFF Power (TOOP) Measurement.

SETup:TOOPower:CONTinuous

Function

Sets/queries the trigger arm state for the Transmit ON/OFF Power measurement. The trigger arm state determines whether the Transmit ON/OFF Power measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)).

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETUP:TOOPower:CONTINUOUS OFF"

SETup:TOOPower:COUNt[:SNUMber]

Function

The setting form of this command performs two functions: (1) sets the number of Transmit ON/OFF Power measurements to be made in a multi-measurement, and (2) sets the multi-measurement STATe command to 1 (on).

The query form returns the number of Transmit ON/OFF power measurements to be made when multi-measurement state is ON.

Setting

Range:1 to 999

Query

Range:1 to 999

*RST Setting

OFF (10 when STATe = ON)

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:COUNt 5"

SETup:TOOPower:COUNt:NUMBer

Function

Sets/queries the number of Transmit ON/OFF power measurement to be made when the multi-measurement state is set to ON.

Setting

Range: 1 to 999

Query

Range: 1 to 999

*RST Setting

10

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETUP:TOOPower:COUNT:NUMBER 5"

SETup:TOOPower:COUNt:STATe

Function

Sets/queries the Transmit ON/OFF Power multi-measurement state.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:COUNt:STATe ON"

SETup:TOOPower:LIMit

Function

Sets/queries the OFF power mask limits for each range. There are three parameters (separated by comma) for this command, representing the mask limit for Range1, Range 2, Range 3 respectively.

Setting

For each of the three parameters:

  • Range: -80 to +30 dBm

  • Resolution:0.01

Query

Same as setting

*RST Setting

-65.0,-50.0,-65.0

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:LIMit -65.0,-50.0,-65.0"

SETup:TOOPower:OFFPower:MODE

Function

Sets/queries the way to get the power result of the three ranges. This parameter can be set to either Average or Worst. If it is set to Average, the power result for each range is the average chip power of the range; If it is set to Worst, the power result for each range is the highest chip power in the range.

Note: If the highest power of the mobile phone can reach as much as -65 dBm, It is recommended that you use Average as the OFF power mode. Otherwise the measurement may be easily to fail.

Setting

Range: AVERage |WORSt

Query

Range: AVER|WORS

*RST Setting

AVERage

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:OFFPower:MODE AVERage"

SETup:TOOPower:TIME[:OFFSet]

Function

Sets/queries the measurement offsets. These offsets determine which chip results will be retrieve by FETCh:TOOPower:TIME:POWer?.  Up to 12 offsets are set/returned in the form of an array (separated by comma).

Setting

An array of up to 12 offset values separated by comma. For each of the offsets:

  • Range:  -864 to 1711

  • Resolution: 1 (chip)

Query

Same as setting

*RST Setting

-160,-100,-34,-33,-14,-1,0,847,848,860,1200,1711

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:TIME:OFFSet -160,-100,-34,-33,-14,-1,0,847,848,860,1200,1711"

SETup:TOOPower:TIMeout[:STIMe]

Function

The setting form of this command performs two functions: (1) sets the Transmit ON/OFF Power measurement's timeout value, and (2) sets the Transmit ON/OFF Power measurement's timeout state to 1 (on).

The query form returns the Transmit ON/OFF Power measurement's timeout value.

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Unit: S | MS | US | NS

Query

Range: 0.1 to 999.9

*RST Setting

10 seconds

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:TIMeout 5S"

SETup:TOOPower:TIMeout:STATe

Function

Sets/Queries the Transmit ON/OFF Power measurement's timeout state.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

 0(OFF)

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:TIMeout:STATe ON"

SETup:TOOPower:TIMeout:TIME

Function

Sets/queries the Transmit ON/OFF Power measurement's timeout.

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Unit: S | MS | US | NS

Query

Range: 0.1 to 999.9

*RST Setting

10 s

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:TIMeout:TIME 5S"

SETup:TOOPower:TRACe[:STATe]

Function

Sets/queries whether the whole trace results are available.

Setting

Range: ON | OFF | 0 | 1

Query

Range: 0|1

*RST Setting

OFF

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETup:TOOPower:TRACe ON"

SETup:TOOPower:TRIGger:DELay

Function

Sets/queries the Transmit ON/OFF Power measurement's trigger delay setting.

Setting

Range:-10 to 10 ms

Resolution: 0.1 us

Unit: S | MS | US | NS

Query

Same as setting

*RST Setting

0 s

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETUP:TOOPower:TRIGGER:DELAY 0MS"

SETup:TOOPower:TRIGger:SOURce

Function

Sets/queries the Transmit ON/OFF Power measurement's Trigger Source.

Setting

Range: AUTO | IMMediate | RISE |EXTernal | PROTocol

Query

Range: AUTO | IMM | RISE |EXT| PROT

*RST Setting

AUTO

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"SETUP:TOOPower:TRIGGER:SOURCE AUTO"