CALL:DPCHannel

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

CALL[:CELL]:DPCHannel:LEVel

Function

Sets/queries the DL DPCH level offset.

The function is used in active cell operating mode.

Setting

Range:-30.00 dB to 0 dB

Resolution:0.01

Query

Same as setting

*RST Setting

0dB

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:DPCHannel:LEVEL -7"

CALL[:CELL]:DPCHannel:STATe   

Function

Sets/queries the DL DPCH level state.

The function is used in active cell operating mode.

Setting

Range:On|Off

Query

Range:1|0

*RST Setting

On

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:DPCHannel:STATe ON"

CALL[:CELL]:DPCHannel[:SLEVel]  

Function

The setting form of this command performs two functions: (1) sets the DL DPCH level and (2) sets DL DPCH level state to on. The query form of this command returns the  DL DPCH level.

The function is used in active cell operating mode.

Setting

Range:-30.00 dB to 0 dB

Resolution:0.01

Query

Same as setting

*RST Setting

0dB

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:DPCHannel -7"

CALL:DPCHannel:ORTHogonal:LEVel?

Function

Queries the calculated DPCHo Power level.

Query

returned value

*RST Setting

9.91E37

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"CALL:DPCHannel:ORTHogonal:LEVel?"

CALL:DPCHannel:ORTHogonal:STATe?

Function

Queries the calculated DPCHo Power State.

Query

0|1

*RST Setting

1

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"CALL:DPCHannel:ORTHogonal:STATe?"

CALL:DPCHannel:TYPE

Function

THIS COMMAND IS OBSOLETE. Please use the CALL:SERVice:RBTest:RAB command to set/query channel type.

Sets/queries the Channel Type setting.

Setting

Range: SRMC12 | MRMC12

Query

same as setting

*RST Setting

SRMC12

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"CALL:DPCHannel:TYPE SRMC12"