The test set supports both IPv4 and IPv6 for IP connection. This page describes how to set up the IP parameters and get the IP information of the test set.
See the related topics at the bottom of this page on how to configure the LAN of the test set, the IPv4 and IPv6 addressing requirements.
 
Manual Operation: 
Instrument IP Info
 can be accessed by first pressing the 
SYSTEM CONFIG
 hardkey, go to 
Control 2 of 2
 for the 
Instrument IP Info 
(F3)
, and then press 
Instrument IP Setup
 for the 
Instrument IP Setup
 menu. Besides, 
LAN IP Address
, 
LAN IP Address 2 (Data+)
, 
Subnet Mask
 and 
Default Gateway
 in the Instrument IP Setup menu can also be accessed through 
Instrument Setup
 in 
Control 1 of 2 of 
SYSTEM CONFIG
.
 
A typical display for the 
Instrument Setup
 menu and the 
Instrument IP Addressing
 screen is shown as below:
 
You can view the configured or derived IP information of the test set on the 
Instrument IP Addressing
 screen.
Instrument IP Addressing
 screen, the IPv6 address (IID) for the LAN and LAN 2 are both derived from the MAC address of the test set. Besides, the 
IPv6 Link Local Prefix
 is showed as a fixed value.OUTPUT 714;"SYSTem:COMMunicate:LAN:SELF:ADDRess '130.015.156.255'"
OUTPUT 714;"SYSTem:COMMunicate:LAN:SELF:ADDRess2 '130.015.156.255'"
OUTPUT 714;"SYSTem:COMMunicate:LAN:SELF:SMASK '255.2.6.200'"
OUTPUT 714;"SYSTem:COMMunicate:LAN:SELF:DGATEWAY '130.2.6.200'"
 
This parameter is an 8-digit number in hexadecimal which sets the upper or the lower part of the IPv6 prefix. The full-length IPv6 prefix is showed in the 
Instrument IP Addressing
 screen.
If you leave this parameter blank, the test set will assign an all-zero IPv6 address prefix and an error will be displayed. You can only change the IPv6 prefix when the data connection status is Idle.
 
You are not allowed to change the IPv6 prefix of the test set if the 
IPv6 Router State
 is 
. 
On
This parameter is stored in the test set's non-volatile RAM and is not affected by power cycle, full preset or save/recall operations. GPIB example:
OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:8960:8960:8960'"
 
The IPv6 Default Router Interface ID identifies the IPv6 default Router to which the test set sends packets. This is similar to the Default Gateway in IPv4. This parameter is an 8-digit number in hexadecimal which sets the upper or the lower part of the IPv6 Default Router Interface ID. The full-length IPv6 Default Router Interface ID is shown in the 
Instrument IP Addressing
 screen. GPIB example:
OUTPUT 714;" SYSTem:COMMunicate:LAN:DGATeway:IP6:IID '0000:0000:821D:B001'"
This setting is only applicable to the lab application .
This setting enables or disables the IPv6 router state of the test set.
 
If the IPv6 Router State is set to 
On
, the test set acts as an IPv6 router, and the IPv6 servers in the same IPv6 segment will use it as a default IPv6 router to send the IPv6 packets. The 
IPv6 Router State
 is set to Off by default.
 
Operating Considerations: When you don't need the test set to be an IPv6 router, it is strongly recommended you set the 
IPv6 Router State
 to 
Off
. This is because if it is left On, the test set periodically broadcasts a Router Advertisement (RA) message and declares to the whole subnet that it is the default IPv6 router of the subnet. Turning it off can avoid the potential interference of the IPv6 routers and hosts in the same subnet. Besides, very quick back-and-forth operations (for instance a quick On-Off-On switching) is not recommended for this setting.
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ROUTER:STATE:IP6 ON"