| Sets/queries the test set's GPIB address. Configuring the Test Set's GPIB | |
|
14 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
|
OUTPUT 714;"SYSTEM:COMMUNICATE:GPIB:SELF:ADDRESS 14" ! Sets the GPIB address to 14. |
|
|
Sets/queries the test set's SCPI debugger state. When the state is on; enhanced error messages (generated from GPIB commands with syntax errors) are shown the test set display. The error message is printed along with the syntax. <ERR> is displayed at the end of the incorrect node. Non-printable characters will be replaced with the $ symbol. See Error Messages for a list of the errors. The debugger state should be set to on only during GPIB code development. Test times will increase if the debugger state is left on. |
|
| Range: 0|OFF | 1|ON | |
| Query | 0|1 |
OUTPUT 714;"SYSTEM:COMMUNICATE:GPIB:DEBUG:STATE ON" ! Sets debugger to on. |
|
|
Sets/queries the test set's LAN IPv4 address. The value of A is used to determine the subnet mask, see SYSTem:COMMunicate:LAN[:SELF]:SMASk[:IP4] . If the LAN IP address is changed the subnet mask should be checked to insure that it is set to the proper class for that LAN address. (See Configuring the Test Set's LAN ) The LAN IP address cannot be changed when CALL[:CELL]:OPERating:MODE is set to CALL. |
|
|
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B,C, D = 0 to 255 (no embedded spaces). |
|
|
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B,C, D = 0 to 255 (no embedded spaces). |
|
|
0.0.0.0 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
|
| Configuring the Test Set's LAN | |
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ADDRESS '130.015.156.255'" !Sets the LAN IP address. |
|
|
Sets/queries the test set's IPv6 address prefix. See Instrument IP Info/Instrument IP Setup . |
|
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers.
Double-colon "::" can be used in the IPv6 address as valid. Moreover, "::" can be suffixed at the end of the 19 characters which is also a valid IPv6 address prefix. For example: 2009:1:2:3 and 2009:1:2:3:: are all valid IPv6 address prefixes for the GPIB parameter setting. |
|
| Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. | |
| *RST Setting | "" (Null) |
| Requirements | Lab Application Revision: F.00.19 and above |
OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:8960:8960:8960'" !Sets the IPv6 address prefix to 2009:8960:8960:8960. OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3'" !Sets the IPv6 address prefix to 2009:1:2:3. OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3::'" !Sets the IPv6 address prefix to 2009:1:2:3::. |
|
|
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B.C. D = 0 to 255 (no embedded spaces). |
|
|
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B,C, D = 0 to 255 (no embedded spaces). |
|
|
0.0.0.0 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
|
| LAN 2 PORT | |
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ADDRESS2 '130.015.156.255'" ! Sets the LAN 2 IP address. |
|
|
Sets/queries the test set's IPv6 Default Router Interface ID. See Instrument IP Info/Instrument IP Setup for details. |
|
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers. Double-colon "::" can be used in the IPv6 Default Router Interface ID as valid. Moreover, "::" can be prefixed at the beginning of the 19 characters which is also a valid IPv6 Default Router Interface ID. For example: 8960::1, ::1:2 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. The IPv6 Default Router Interface parameter is also IPv4 address-compatible with the format: ::W.X.Y.Z, where W.X.Y.Z is the dotted decimal representation of an IPv4 address. For example, ::8960:8960:146.208.232:220 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. |
|
| Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. | |
| *RST Setting | "" (Null) |
| Requirements | Lab Application Revision: F.00.19 and above |
OUTPUT 714;" SYSTem:COMMunicate:LAN:DGATeway:IP6:IID '0000:0000:821D:B001'" !Sets the test set's IPv6 Default Router Interface ID to 0000:0000:821D:B001. |
|
| Sets/queries whether the test set acts as a IPv6 router. See IPv6 Router State . | |
| *RST Setting | Off |
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ROUTER:STATE:IP6 Off" !Sets the IPv6 Router State to "off" |
|
| Sets/queries the external Evolved Packet Core (EPC) simulator's IPv4 address. See Ext EPC IP Addr . | |
| Same as setting | |
| *RST Setting | "0.0.0.0" (Null) |
OUTPUT 714;"SYSTem:COMMunicate:LAN:EPCore:ADDRess '130.015.156.235'" !Sets the external Evolved Packet Core (EPC) simulator's IPv4 address to '130.015.156.235'. |
|
| Initiates the Connect to External EPC immediate action. See Connect To External EPC . | |
OUTPUT 714;"SYSTem:COMMunicate:LAN:EPCore:CONNect" !Initiates a connection to the External EPC simulator. |
|
| Initiates the Disconnect From External EPC immediate action. See Disconnect From External EPC . | |
OUTPUT 714;"SYSTem:COMMunicate:LAN:EPCore:DCONnect" !Disconnect the test set from the External EPC simulator. |
|
|
Sets/queries the External 8960 IP Address . |
|
|
Range: 15 characters formatted as follows: A.B.C.D where A= 0 to 126 and 128 to 223, B.C.D = 0 to 255 (no embedded spaces), blank field. |
|
|
Range: 15 characters formatted as follows: "A.B.C.D" where A= 0 to 126 and 128 to 223, B.C.D = 0 to 255 (no embedded spaces), "". |
|
|
"" (this parameter is not affected by any reset operation and can only be changed by direct user access) |
|
|
Lab Application Revision: C.01 and above Test Application Revision: A.06 and above, with the required feature license |
|
OUTPUT 714;"SYSTem:COMMunicate:LAN:EXTernal:ADDRess '130.015.156.255'" ! Sets the External 8960 IP Address. |
|
Initiates the
Connect to External 8960
immediate action (see
External Device Connection
). |
|
|
Lab Application Revision: C.01 and above Test Application Revision: A.06 and above, with the required feature license |
|
OUTPUT 714;"SYSTem:COMMunicate:LAN:EXTernal:CONNect" |
|
Initiates the
Disconnect from External 8960
immediate action (see
External Device Connection
). |
|
|
Lab Application Revision: C.01 and above Test Application Revision: A.06 and above, with the required feature license |
|
OUTPUT 714;"SYSTem:COMMunicate:LAN:EXTernal:DCONnect" |
|