Last updated: January 15, 2009
This section is only applicable to the lab applications.
Please keep in mind that an HTTP address requires all the components shown in the URL below, and that this section focuses on the request URL portion of the address. See HTTP Overview for more information regarding other components of the HTTP address.
If you wish to use the HTTP interface to configure and send cell broadcast messages to the mobile station attached to the test set's RF port, you must do the following:
Once the HTTP interface is enabled (see Enable the Test Set's HTTP Interface ), you can do the following through the HTTP interface:
You can do this by sending an HTTP command to the test set with the following request URL format:
If the cell broadcast format started successfully, the following message is displayed in your internet browser:
You can do this by sending an HTTP command to the test set with the following request URL format:
If the cell broadcast format started successfully, the following message is displayed in your internet browser:
When using the HTTP interface in the test set for sending cell broadcast messages, you must configure a request URL.
Requests to send cell broadcast messages to the mobile station attached to the test set using the HTTP interface must be configured using the following rules:
/cbsms/message<n>/?parameter1=value1¶meter2=value2¶meter3=value3......
The parameters and values variables provides the content of the cell broadcast message as well as additional information for header configuration and test set configuration. All configurable parameters and values are detailed in Request URL Parameters .
Both POST and GET HTTP requests are accepted by the test set for sending cell broadcast messages.
If POST is used as the request method, the URL request parameters detailed in Request URL Parameters are not included in the request URL, but are included in the request body instead. Therefore, the request URL in POST requests contains only `cbsms/message<n>' (when <n> must be a 1, 2 or 3).
| Parameter | Use and expected value | Inclusion |
|---|---|---|
| CODE | Specifies the 10-bit message code element of the cell broadcast message's serial number.Expected value: decimal number in the range 0-1023 |
Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:CODE . |
| DATA | Specifies the binary data to be sent in the message.Expected value: 0-2460 length character string of ASCII formatted hexadecimal characters |
Optional -This parameter cannot be included in the same request as the TEXT parameter. Including this parameter affects the settings for CALL:SMService:CBRoadcast:MESSage[<n>]:CONTent and CALL:SMService:CBRoadcast:MESSage[<n>]:CDATa . |
| DCS | Specifies the 8-bit data coding scheme of the cell broadcast message.Expected value: Decimal number in the range 0-255 |
Optional -This parameter cannot be included in the same request as the DCSHEX parameter. (default*= 1) Including this parameter affects the settings for CALL:SMService:CBRoadcast:MESSage[<n>]:DCSCheme[:SPECify] and CALL:SMService:CBRoadcast:MESSage[<n>]:DCSCheme:VALue . |
| DCSHEX | Specifies the 8-bit data coding scheme of the cell broadcast message.Expected value: string of hex characters in the range 0 - FF |
Optional -This parameter cannot be included in the same request as the DCS parameter. (default*= not used). Including this parameter affects the settings for CALL:SMService:CBRoadcast:MESSage[<n>]:DCSCheme[:SPECify] and CALL:SMService:CBRoadcast:MESSage[<n>]:DCSCheme:VALue . |
| GSCOPE | Specifies the 2-bit geographical scope element of the cell broadcast message's serial number.Expected value: decimal number in the range 0-3 |
Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:GSCope . |
| ID | Specifies the 16-bit message identifier of the cell broadcast message.Expected value: Decimal number in the range 0-65535 |
Optional -This parameter cannot be included in the same request as the IDHEX parameter. (default*= 0) Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:IDENtifier . |
| IDHEX | Specifies the 16-bit message identifier for the cell broadcast message.Expected value: String of hex characters in the range 0 - FFFF |
Optional -This parameter cannot be included in the same request as the ID parameter. (default*= not used) Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:IDENtifier . |
| REPETITION | Specifies the repetition period for the message in seconds. This parameter may be included in HTTP requests to configure any of the individual cell broadcast messages however the associated value is be applied to ALL of the messages regardless of which message the HTTP request was for.Expected value: Decimal number in the range 1 - 1800 |
Optional -This parameter cannot be included in the same request as the REPUNITS parameter. (default*= 30) Including this parameter affects the setting for CALL:SMService:CBRoadcast:REPetition[:SEConds] . |
| STATE | Specifies if the message should be transmitted when the cell broadcast service is running.Expected value: Decimal number in the range 0 - 1 where 0=OFF, 1=ON. |
Optional (default*: Message 1=ON, Message 2 and 3 = OFF) Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:STATe . |
| TEXT |
Specifies the text to be sent in the message. Expected Value: 0 to 1395 length character string of 7-bit text characters. |
Optional -This parameter cannot be included in the same request as the DATA parameter. Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:CONTent and CALL:SMService:CBRoadcast:MESSage[<n>]:CTEXt . |
| UPDATE | Specifies the 4-bit update number element of the cell broadcast message's serial number.Expected value: Decimal number in the range 0-15 |
Including this parameter affects the setting for CALL:SMService:CBRoadcast:MESSage[<n>]:UPDate . |
|
*This value is the setting for the parameter when the test set is powered on. If a parameter is not included, the setting for the parameter does not revert to the default settings, but retains the current parameter settings. |
||
To send a text based cell broadcast message with the following message details:
you would format the cell broadcast HTTP request URL as follows:
/cbsms/message1/?GEOSCOPE=3&CODE=5&UPDATE=1&ID=2&DCS=1&TEXT=This%20is%20a%20text%20message%20for%20message%20one&REPETITION=10
To send a binary message with the following message details:
you would format the cell broadcast message as follows:
/cbsms/message2/?GEOSCOPE=1&CODE=13&UPDATE=1&ID=6&DCS=245&DATA=014FA553000FF110&STATE=1
Messages can be updated over HTTP while the cell broadcast service is enabled and running. For example, if message 1 and message 2 are configured as described in Example Text Cell Broadcast Request URL and Example Binary Cell Broadcast Request URL and you wish to change the contents of the text message sent in message 1 to "This is an updated text message for message one", you would send the following URL:
/cbsms/message1/?TEXT=This%20is%20an%20updated%20text%20message%20for%20message%20one&UPDATE=2
Notice that the update number has changed from 1 to 2 to indicate to the mobile station that the contents of the message have been altered.
If you wish to stop transmitting message 2, you would send the following URL: