Last updated: January 15, 2009
This section is only applicable to the lab applications.
The test set provides the delivery status of mobile terminated SMS messages on the front panel, or it is accessible via the GPIB or HTTP interfaces.
There are six possible MT SMS message states.
The CALL:SMService:PTPoint[:MTERminated]:SEND:STATe? query returns a string indicating the state of the last message sent from the test set to the mobile station.
If the delivery status returned is "REJ", you can use the CALL:SMService:PTPoint[:MTERminated]:RCAuse? query to retrieve the reject cause value returned by the mobile station. See Reject Cause for the meanings of the possible cause values.
The state of the last MT SMS message sent from the test set to the mobile station can be queried from the test set using an HTTP GET request with the following URL:
The delivery state is returned in the body of the HTTP response.
You can query the MT SMS delivery state through the HTTP interface using an internet browser by entering the following URL:
where <x.x.x.x> is the IP address of the test set sending the SMS to the mobile station. This example is illustrated in the following figure.
If the state returned is "REJ", the body of the HTTP response also contains the reject cause value as an integer. The reject cause value is placed in the response body after the REJ characters and separated from them by a single space character. For example, "REJ 211" is returned in the HTTP response if the MT SMS was rejected with a cause value of 211. See the following figure.
See Reject Cause for the meanings of the possible cause values.
| Reject Cause | Hex equivalent | Description |
|---|---|---|
| 129 | 81 | Short message Type 0 not supported |
| 130 | 82 | Cannot replace short message |
| 143 | 8F | Unspecified TP-PID error |
| 145 | 90 | Message class not supported |
| 159 | 9F | Unspecified TP-DCS error |
| 176 | B0 | TPDU not supported |
| 208 | D0 | (U)SIM SMS storage full |
| 209 | D1 | No SMS storage capability in (U)SIM |
| 210 | D2 | Error in MS |
| 211 | D3 | Memory Capacity Exceeded |
| 212 | D4 | (U)SIM Application Toolkit Busy |
| 213 | D5 | (U)SIM data download error |
| 224-254 | E0-FE | Values specific to an application |
| 255 | FF | Unspecified error cause |