Show 

Home > Compressed Mode Ladder Diagrams



Compressed Mode Ladder Diagrams

Compressed Mode Ladder Diagrams

Last updated: January 15, 2009

This section is only applicable to the lab application.

There are four different ways that compressed mode can be enabled in the test set and UE (see Summary of Options for Enabling Compressed Mode and UE Measurements ).

TGPS Definition during Call Setup, Compressed Mode Activated without UE Measurements

TGPS Definition after Call Is Established, Compressed Mode Activated without UE Measurements

TGPS Definition during Call Setup, Compressed Mode Activated with UE Measurements

TGPS Definition after Call Is Established, Compressed Mode Activated with UE Measurements

Deactivating Compressed Mode

Related Topics


Compressed Mode