Call Processing Ladder Diagrams

Call Processing Ladder Diagrams

Last updated: January 15, 2009

The following diagrams illustrate the procedures used by the test set for several key call processing operations.

RRC Connection Setup Procedure

   

Location Update (Registration) Procedure

   

Paging Procedure

   

Radio Bearer Test Mode Origination to CELL_DCH - CS Domain (Non-HSPA or HSDPA)

See 3GPP TS 34.108 s7.3.2.3 "For UE supporting CS"

   

Radio Bearer Test Mode Origination to CELL_DCH - PS Domain (HSDPA)

See 3GPP TS 34.108 s7.3.2.3 "For UE supporting PS only"

   

Radio Bearer Test Mode Origination to CELL_DCH - CS/PS Domain (HSDPA or HSPA)

   

Radio Bearer Test Mode Origination to CELL_FACH

   

BS Release from Radio Bearer Test Mode in CELL_DCH

   

BS Release from Radio Bearer Test Mode in CELL_FACH

Related Topics


W-CDMA Concepts

Base Station Originated Call Setup Flowchart

Security Ladder Diagrams