Last updated: January 15, 2009
This section is only applicable to the lab application.
This procedure details how to set up the two-cell test system.
All of the procedures in this section require that you first set up the two-cell test system as follows:
External Device Connection
.
Amplitude Offset
for each test set.
DUT IP Address
to a different value in each test set.
DUT IP Address
is accessible from
DUT PDP Setup
(
F2
). In the W-CDMA/HSPA application,
DUT IP Address
is accessible from
DUT IP Setup
(
F2
).
Operating Mode
(
F1
) to
Cell Off
.
Cell Band
to the proper value for your mobile, then set
Broadcast Chan
to a different value in each test set (
BCH Parameters
(
F7
)).
Traffic Channel
and PDTCH
Traffic Channel
to a different value in each test set (
TCH Parameters
(
F8
) and
PDTCH Parameters
(
F9
)).
Cell Identity
,
LAC
,
RAC
,
NCC
and
BCC
to a different value in each test set (
Cell Info
(
F6
),
Cell Identification
(
F3
)).
Persistent Attach State
to
On
in both test sets (
Cell Info
(
F6
),
Cell Operation
(
F1
)).
IMSI Attach State
to
On
in both test sets (
Cell Info
(
F6
),
Cell Parameters
(
F1
)).
Cell Info
(
F6
),
Cell Lists
(
F4
):
GSM Neighbours (BCH)
(
F1
), set
Cell State
to
On
and set
Neighbor Cell 1 ARFCN
,
NCC
and
BCC
to match the
Broadcast Chan
,
NCC
and
BCC
settings in the other test set (if both test sets are emulating a GSM/GPRS/EGPRS cell).
3G FDD Neighbors
(
F4
), set
UARFCN State
to
On
and set
UARFCN
and
Cell 1 Scrambling Code
to match the
DL Channel
and
Primary Scrambling Code
settings in the other test set (if the other test set is emulating a W-CDMA/HSPA cell).
Cell Parameters
as desired to affect the cell selections/reselections (
Cell Info
(
F6
)).
Network Control Order
to
0
or
1
(
Measurement Reports
(
F6
),
Configure
(
F2
),
General Meas Parameters
(
F1
)).
Cell Power
(
F7
) as desired (
BCH Parameters
(
F7
)).
Data Connection Type
(
F2
) is set to
Auto
in both test sets.
Operating Mode
(
F1
) to
Active Cell (GSM)
,
Active Cell (GPRS)
or
Active Cell (EGPRS)
as desired in each test set.
Operating Mode
(
F1
) to
Cell Off
.
DL Channel
to the proper value for your mobile (
Channel (UARFCN) Parms
(
F12
).
Primary Scrambling Code
as desired (
Generator Info
(
F3
),
Downlink Channel Codes
(
F2
),
Shared Channel Codes
(
F2
)).
SIB11 Cell Info List
(
F3
):
LAC
,
RAC
and
Cell Identity
to different values from the other test set, and set
ATT (IMSI Attach) Flag State
to
Set
(
Cell Info
(
F2
),
Cell Parameters
(
F1
)).
Cell Parameters
,
Reselection Parameters
and
Access Restriction Parameters
as desired to affect the cell selections/reselections (
Cell Info
(
F2
)).
Cell Power
(
F7
) as desired.
GPRS Radio Access Bearer
as desired (
Data Channels
(
F4
),
Packet Data Setup
(
F1
)).
Operating Mode
(
F1
) to
Active Cell
.This procedure allows you to observe which cell the mobile selects from the two-cell test system once it has completed its power-up sequence.
This procedure assumes that you have Set Up the Two-Cell Test System , the mobile has been powered on and is camped on one of the cells in the system as is described in the Mobile-initiated Cell Selection procedure.
Note, mobile-initiated cell reselection is not possible from a W-CDMA/HSPA cell when the mobile is PDP active. If you turn off the serving W-CDMA/HSPA test set's cell power, the mobile will find the other test set and establish a PDP Context with it; however, this is not the same as a mobile-initiated reselection to the other test set.
Cell Power
of one or both of the test sets so that the test set that was not initially selected has a much stronger signal (or simply turn the cell power off in the test set the mobile is currently camped on).This procedure assumes that you have Set Up the Two-Cell Test System and the mobile has been powered on and is camped on one of the cells in the system as is described in the Mobile-initiated Cell Selection procedure.
Note, mobile-initiated cell reselection is not possible from a W-CDMA/HSPA cell when the mobile is PDP active. If you turn off the serving W-CDMA/HSPA test set's cell power, the mobile will find the other test set and establish a PDP Context with it; however, this is not the same as a mobile-initiated reselection to the other test set.
Operating Mode
and
Coding Scheme
for GPRS/EGPRS or the
GPRS Radio Access Bearer
and
CQI Value
for W-CDMA/HSPA).
Data Throughput Monitor
on both test sets. Observe the transfer of data on the current serving cell. You can also observe the DUT IP counters present on the
Call Setup
screen in GPRS/EGPRS or on the
Data Channels
screen in W-CDMA/HSPA.
Cell Power
of one or both of the test sets so that the test set that was not initially selected has much stronger signal (or simply turn the cell power off in the test set the mobile is currently camped on).
Data Throughput Monitor
display and IP counters on both test sets.This procedure explains how to test both idle mode and packet-switched data transfer mode cell reselections. This procedure assumes that you have Set Up the Two-Cell Test System and the mobile has been powered on and is camped on one of the cells in the system as is described in the Mobile-initiated Cell Selection procedure. No CS voice call should be connected in this procedure.
Note, in a W-CDMA/HSPA cell, for Release 99 mobiles, network-initiated cell reselection is only possible when the mobile is PDP active.
Data Throughput Monitor
.
Handover Parameters
(
F10
),
Ext Handover Setup
(
F9
). If the current serving cell is W-CDMA/HSPA, select
Handovers
(
F5
),
1 of 2
(
MORE
),
External 8960 Handover
(
F1
).
Note: The external handover menus are only available if the two test sets currently have an
External Device Connection
. This can be verified by observing the
External Device Connection Setup
screen (
SYSTEM CONFIG
,
More
(
1 of 2
),
External Device Connection
(
F4
)), or the
ExtDev
status indicator in the
Instrument Status Area
:
Ext Handover Execute
or
Execute Ext 8960 Handover
(
F5
). This instructs the network to send a PCCO message if the current serving cell is GPRS/EGPRS or a CCO message if the current serving cell is W-CDMA/HSPA.
Data Throughput Monitor
display and IP counters on both test sets (for PS data transfer mode cell reselection).
This procedure only applies to CS (Circuit-Switched) voice and DTM (Dual Transfer Mode) handovers. This procedure assumes that you have Set Up the Two-Cell Test System and the mobile has been powered on and is camped on one of the cells in the system as is described in the Mobile-initiated Cell Selection procedure.
Note, because simultaneous services in the W-CDMA/HSPA application do not support two-cell test system handovers, perfoming a handover from a GSM/GPRS/EGPRS DTM connection to a W-CDMA/HSPA cell is unsupported, and may result in undetermined behavior.
Connected
(for a DTM connection, the connection status window displays the voice and data connection status in the form: voice/data).
Handover Parameters
(
F10
),
Ext Handover Setup
(
F9
). If the current serving cell is W-CDMA/HSPA, select
Handovers
(
F5
),
1 of 2
(
MORE
),
External 8960 Handover
(
F1
).
Note: The external handover menus are only available if the two test sets currently have an
External Device Connection
. This can be verified by observing the
External Device Connection Setup
screen (
SYSTEM CONFIG
,
More
(
1 of 2
),
External Device Connection
(
F4
)), or the
ExtDev
status indicator in the
Instrument Status Area
:
Ext Handover Execute
or
Execute Ext 8960 Handover
(
F5
). This instructs the network to begin its handover procedure.
Handover
. The destination test set then transitions to
Connected
, while the originating test set transitions to
Idle
.Troubleshooting the Two-Cell Test System