|
Sets/queries the HS-PDSCH Second Code Support. The standard specifies that at most two predefined HS-PDSCH codes are assigned per UE for HS-SCCH-less operation. The four comma-separated value indicates whether the second HS-PDSCH code will be used for the corresponding TB size indexed by CALL:CPC:HLESs:TBSize:INDex . "1" means that two HS-PDSCH codes will be used for the corresponding transport block, otherwise only one HS-PDSCH code will be used. This setting is only applicable when the Current HS-SCCH-less Activated State is On and the HS-DSCH Transmission Type is "HS-SCCH-less". |
|
| 4 comma separated values in the range: 1|0 | |
| 4 comma separated values in the range: 1|0 | |
| *RST Setting | 0, 0, 0, 0 |
| Requirements | |
OUTPUT 714;"CALL:CPC:HLESs:HSPDschannel:CODE 0, 0, 0, 0" |
|
|
This parameter controls which cell is used to send the HS-SCCH Order to activate/deactivate the DTX and DRX based on DTX Order Info and DRX Order Info . |
|
| Same as setting | |
|
Test Application Revision: A.19.00 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CPC:HSSCchannel:ORDer:FROM SSCell" !Sets the Secondary Serving Cell to send the HS-SCCH Order to activate/deactivate the DTX and DRX. |
|
|
Perform the Send HS-SCCH Order action. |
|
| Lab Application Revision: F.00.19 and above | |
OUTPUT 714;"CALL:CPC:HSSCchannel:ORDer:SEND" !Initiates a Send HS-SCCH Order. |
|
| *RST Setting | |
| Requirements | Lab Application Revision: F.00.19 and above |
OUTPUT 714;"CALL:CPC:STATe OFF" ! Sets CPC State to Off. |
|