Last updated: January 14, 2010
This section is only applicable to the lab application or feature-licensed test application.
|
THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel[1]:CCODe:CODE . Sets/queries the HS-SCCH 1 Channelization Code . |
|
| Same as setting. | |
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel:CCODe CODE11" ! Sets the HS-SCCH 1 Channelization Code to 11. |
|
|
Sets/queries the HS-SCCH 1 Channelization Code . This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter). |
|
| Same as setting. | |
|
Lab Application Revision: F.00 and above Test Application Revision: A.14 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel:CCODe:CODE 2" ! Sets the HS-SCCH 1 Channelization Code to 2. |
|
|
THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel2:CCODe:CODE . Sets/queries the HS-SCCH 2 Channelization Code . |
|
| Same as setting. | |
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel2:CCODe CODE11" ! Sets the HS-SCCH 2 Channelization Code to 11. |
|
|
Sets/queries the HS-SCCH 2 Channelization Code . This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter). |
|
| Same as setting. | |
|
Lab Application Revision: F.00 and above Test Application Revision: A.14 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel2:CCODe:CODE 6" ! Sets the HS-SCCH 2 Channelization Code to 6. |
|
|
THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel3:CCODe:CODE . Sets/queries the HS-SCCH 3 Channelization Code . |
|
| Same as setting. | |
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel3:CCODe CODE11" ! Sets the HS-SCCH 3 Channelization Code to 11. |
|
|
Sets/queries the HS-SCCH 3 Channelization Code . This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter). |
|
| Same as setting. | |
|
Lab Application Revision: F.00 and above Test Application Revision: A.14 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel3:CCODe:CODE 9" ! Sets the HS-SCCH 3 Channelization Code to 9. |
|
|
THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel4:CCODe:CODE . Sets/queries the HS-SCCH 4 Channelization Code . |
|
| Same as setting. | |
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel4:CCODe CODE11" ! Sets the HS-SCCH 4 Channelization Code to 11. |
|
|
Sets/queries the HS-SCCH 4 Channelization Code . This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter). |
|
| Same as setting. | |
|
Lab Application Revision: F.00 and above Test Application Revision: A.14 and above, with the required feature license |
|
OUTPUT 714;"CALL:HSSCchannel4:CCODe:CODE 10" ! Sets the HS-SCCH 4 Channelization Code to 10. |
|