Last updated: October 19, 2012
You can specify the channel code, state and level of most of the downlink channels generated by the test set (some are fixed). Some of the downlink channels can have a different code, state or level depending upon the state of the test set.
| Operating Mode | Call State | Connection Type | Codes | |
|---|---|---|---|---|
| FDD Test | FDD Test Operating Mode | |||
| Active Cell | Idle | Shared DL Channel Codes | Downlink Channel Levels | |
| Connected | non-HSDPA/ non-HSPA | Shared DL Channel Codes , WCDMA DL Channel Codes | WCDMA Connected DL Channel Levels | |
| Connected | HSDPA | Shared DL Channel Codes , HSDPA/HSPA DL Channel Codes | HSDPA Connected DL Channel Levels | |
| Connected | HSPA | Shared DL Channel Codes , HSDPA/HSPA DL Channel Codes | HSPA Connected DL Channel Levels | |
Use the Downlink Channel Code Preset to easily configure the 3GPP TS 34.121-1 channel codes from the front panel.
If the sum of the downlink channel levels is less than the cell power setting, Orthogonal Channel Noise Simulator (OCNS) power is automatically added.
Downlink
Channel Codes can not be changed in
Active Cell operating mode (use
Cell Off operating mode to change the active cell downlink
channel codes). The downlink channel codes currently in use are
displayed in the Downlink Code Channel Information
window.
Primary
Scrambling Code
GPIB command: CALL:SCODe
S-CCPCH Channelization Code
The S-CCPCH OVSF (Orthogonal Variable Spreading Factor) is fixed at 64. This parameter cannot be set to 26 when RB Test Mode First HS-PDSCH Channel Code or PS Data First HS-PDSCH Channel Code is set to 5 or 6.
GPIB command: CALL:CCPChannel:SECondary:CCODe:CODE
PICH Channelization Code
The PICH OVSF is fixed at 256.
GPIB command: CALL[:CELL]:PICHannel:CCODe:CODE
AICH Channelization Code
The AICH OVSF is fixed at 256.
GPIB command: CALL:AICHannel:CCODe:CODE
S-CPICH Channelization Code
The S-CPICH OVSF is fixed at 256.
This setting
can not be changed while the Operating
Mode is Active Cell
.
GPIB command: CALL[:CELL[1]]:CPIChannel:SECondary:CCODe:CODE
The CPICH OVSF/channelization code is fixed at 256,0.
The P-CCPCH/SCH OVSF/channelization code is fixed at 256,1.
The method for setting downlink DPCH channel codes differs between the test application and lab application. The following table illustrates the valid channelization codes for each type of DPCH channel, and indicates the GPIB commands and front panel fields used to set the channelization codes, for both the test application and lab application (see How Do I Change Generator Information? to help you find these fields from the front panel).
| Downlink Channel Type | Valid Channelization Code | Test Application Front Panel Setting and GPIB Command |
Lab Application Front Panel Setting and GPIB Command |
|---|---|---|---|
| Signalling Radio Bearers: (see Signalling Radio Bearer (SRB) Parameters ) | |||
| 2.2k DCCH | 12/13/20/21/40/43/ 58/126/127/142/ 153/174/235/255 |
3.4k SRB Channelization Code, CALL:SRBearer |
DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE |
| 3.4k DCCH | 12/13/20/21/40/43/ 58/126/127/142/ 153/174/235/255 |
3.4k SRB Channelization Code, CALL:SRBearer |
DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE |
| 13.6k DCCH | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| Radio Bearer Test Mode Reference Measurement Channels: (see Radio Bearer Test Mode ) | |||
| 12.2k RMC | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 64k RMC | 6/10/12/14/16/18/ 20/22/24/25/26/27 |
DPCH 64k RMC Channelization Code, CALL:DPCHannel:RMC64:CCODe | DPCH 120 ksps (OVSF 32) Channelization Code, CALL:DPCHannel:KSPS120[:CCODe]:CODE |
| 144k RMC | 12/13 | DPCH 144k RMC Channelization Code, CALL:DPCHannel:RMC144:CCODe | DPCH 240 ksps (OVSF 16) Channelization Code, CALL:DPCHannel:KSPS240[:CCODe]:CODE |
| 384k RMC | 6 | DPCH 384k RMC Channelization Code, CALL:DPCHannel:RMC384:CCODe | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| 33k No Coding RMC | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 12.2k UL/64k DL AM RMC | 6/10/12/14/16/18/ 20/22/24/25/26/27 |
DPCH 64k RMC Channelization Code, CALL:DPCHannel:RMC64:CCODe | DPCH 120 ksps (OVSF 32) Channelization Code, CALL:DPCHannel:KSPS120[:CCODe]:CODE |
| 12.2k UL/144k DL AM RMC | 12/13 | DPCH 144k RMC Channelization Code, CALL:DPCHannel:RMC144:CCODe | DPCH 240 ksps (OVSF 16) Channelization Code, CALL:DPCHannel:KSPS240[:CCODe]:CODE |
| 12.2k UL/384k DL AM RMC | 6 | DPCH 384k RMC Channelization Code, CALL:DPCHannel:RMC384:CCODe | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| 64k UL/384k DL AM RMC | 6 | DPCH 384k RMC Channelization Code, CALL:DPCHannel:RMC384:CCODe | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| AMR Radio Access Bearer: (see AMR Setup ) | |||
| 12.2k Voice | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 10.2k Voice | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 7.95k Voice | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 7.4k Voice | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 6.7k Voice | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
DPCH 12.2k RMC & 33k NC RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 5.9k Voice | 12/13/20/21/40/43/ 58/126/127/142/ 153/174/235/255 |
3.4k SRB Channelization Code, CALL:SRBearer |
DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE |
| 5.15k Voice | 12/13/20/21/40/43/ 58/126/127/142/ 153/174/235/255 |
3.4k SRB Channelization Code, CALL:SRBearer |
DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE |
| 4.75k Voice | 12/13/20/21/40/43/ 58/126/127/142/ 153/174/235/255 |
3.4k SRB Channelization Code, CALL:SRBearer |
DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE |
| Circuit Switched Data Radio Access Bearers: (see Circuit Switched Data Service ) | |||
| 14.4k UL/14.4k DL CS Data RAB | 6/9/10/20/29/37/ 45/54/60/63/70/76/ 87/93/112/118 |
Not applicable to the test application. | DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE |
| 57.6k UL/57.6k DL CS Data RAB | 6/10/12/14/16/18/ 20/22/24/25/26/27 |
Not applicable to the test application. | DPCH 120 ksps (OVSF 32) Channelization Code, CALL:DPCHannel:KSPS120[:CCODe]:CODE |
| 64k UL/64k DL CS Data RAB | 6/10/12/14/16/18/ 20/22/24/25/26/27 |
DPCH 64k RMC Channelization Code, CALL:DPCHannel:RMC64:CCODe (feature license required) | DPCH 120 ksps (OVSF 32) Channelization Code, CALL:DPCHannel:KSPS120[:CCODe]:CODE |
| GPRS Radio Access Bearers: (see Packet Switched Data ) | |||
| 64k UL/64k DL PS Data RAB | 6/10/12/14/16/18/ 20/22/24/25/26/27 |
Not applicable to the test application. | DPCH 120 ksps (OVSF 32) Channelization Code, CALL:DPCHannel:KSPS120[:CCODe]:CODE |
| 64k UL/384k DL RMC | 6 | Not applicable to the test application. | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| 64k UL/384k DL PS Data RAB | 6 | Not applicable to the test application. | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| 128k UL/384k DL PS Data RAB * | 6 | Not applicable to the test application. | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
| 384k UL/384k DL PS Data RAB | 6 | Not applicable to the test application. | DPCH 480 ksps (OVSF 8) Channelization Code, CALL:DPCHannel:KSPS480[:CCODe]:CODE |
This section is only applicable to the lab application or feature-licensed test application.
The method for setting downlink DPCH channel codes used during HSDPA and HSPA connections differs between the test application and lab application. The following table illustrates the valid channelization codes for each type of DPCH channel used during HSDPA and HSPA connections, and indicates the GPIB commands and front panel fields used to set the channelization codes, for both the test application and lab application (see How Do I Change Generator Information? to help you find these fields from the front panel).
| Downlink Channel Type | Valid Channelization Codes | Test Application Front Panel Setting and GPIB Command |
Lab Application Front Panel Setting and GPIB Command |
|---|---|---|---|
| Radio Bearer Test Mode Reference Measurement Channels: (see Radio Bearer Test Mode ) | |||
| 12.2k RMC + HSDPA | 20/29/37/45/54 | HSDPA/HSPA DPCH 12.2k RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe:HSDPa | HSDPA/HSPA DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE:HSDPa |
| 20/29/37/45/54 | HSDPA/HSPA DPCH 12.2k RMC Channelization Code, CALL:DPCHannel:RMC12:CCODe:HSDPa | HSDPA/HSPA DPCH 30 ksps (OVSF 128) Channelization Code, CALL:DPCHannel:KSPS30[:CCODe]:CODE:HSDPa | |
| GPRS Radio Access Bearers: (see Packet Switched Data ) | |||
| 3.4k SRB used while on an HSDPA or HSPA packet data connection | 40/43/58 | Not applicable to the test application. | HSDPA/HSPA DPCH 15 ksps (OVSF 256) Channelization Code, CALL:DPCHannel:KSPS15[:CCODe]:CODE:HSDPa |
You can also set the channel code for the following downlink HSDPA and HSPA channels:
Antenna
2 S-CPICH Channelization Code
This setting controls the channelization code of the S-CPICH, which has a spreading factor of 256.
GPIB command: CALL[:CELL[1]]:CPIChannel:SECondary:CCODe:CODE
E-AGCH Channelization Code
This setting controls the channelization code of the E-AGCH. The E-AGCH has a spreading factor of 256.
GPIB command: CALL[:CELL]:EAGChannel:CCODe:CODE
E-HICH/E-RGCH Channelization Code
This setting controls the channelization code of the E-HICH and E-RGCH. These channels have a spreading factor of 128 and by definition use the same channelization code (see 3GPP TS 25.213 s5.2.1). 40 bit signatures are used to provide orthogonality between the two channels (see HSPA Downlink Channel Details ).
GPIB command: CALL[:CELL]:EHIChannel:CCODe:CODE
PS Data First HS-PDSCH Channel Code
This parameter sets the channelization code of the first HS-PDSCH when on an HSDPA packet data connection. If more than one HS-PDSCH is being generated, the other HS-PDSCHs are assigned to the subsequent channelization codes.
This parameter
cannot be set to 5 or 6 when S-CCPCH Channelization
Code is set to 26. Also, the number of HS-PDSCHs specified
by the PS Data HS-DSCH Configuration Type
, when added to the PS Data First
HS-PDSCH Channel Code cannot exceed 15 (otherwise the
HS-PDSCHs would collide with the downlink OCNS channels).
GPIB command: CALL:HSDPa:SERVice:PSData:HSPDschannel:CCODe:CODE
RB Test Mode First HS-PDSCH Channel
Code
This parameter sets the channelization code of the first HS-PDSCH when on an HSDPA RB Test Mode connection. If more than one HS-PDSCH is being generated, the other HS-PDSCHs are assigned to the subsequent channelization codes.
This parameter
cannot be set to 5 or 6 when S-CCPCH Channelization
Code is set to 26. This parameter cannot be set to 5 when HSDPA DPCH 12.2k RMC Channelization
Code is set to 45 or 54, and cannot be set to 6 when HSDPA DPCH 12.2k RMC Channelization
Code is set to 54. Also, the number of HS-PDSCHs specified
by the FRC Type or User
Defined Number of Active HS-PDSCHs settings, when added
to the RB Test Mode First HS-PDSCH
Channel Code cannot exceed 16 (otherwise the HS-PDSCHs
would collide with the downlink OCNS channels).
GPIB command: CALL:HSDPa:SERVice:RBTest:HSPDschannel:CCODe:CODE
HS-SCCH 1 Channelization Code
GPIB command: CALL:HSSCchannel[1]:CCODe:CODE
HS-SCCH 2 Channelization Code
GPIB command: CALL:HSSCchannel2:CCODe:CODE
HS-SCCH 3 Channelization Code
GPIB command: CALL:HSSCchannel3:CCODe:CODE
HS-SCCH 4 Channelization Code
GPIB command: CALL:HSSCchannel4:CCODe:CODE
Secondary Serving Cell PICH Chan Code
GPIB command: CALL:SSCell:PICHannel:CCODe:CODE
PSD Secondary Cell First HS-PDSCH Chan
Code
GPIB command: CALL:HSDPa:SSCell:PSData:HSPDschannel:CCODe:CODE
RBTM Secondary Cell First HSPDSCH Chan
Code
GPIB command: CALL:HSDPa:SSCell:RBTest:HSPDschannel:CCODe:CODE
Secondary Serving Cell HS-SCCH 1 Chan
Code
GPIB command: CALL:SSCell:HSSCchannel1:CCODe:CODE
Secondary Serving Cell HS-SCCH 2 Chan
Code
GPIB command: CALL:SSCell:HSSCchannel2:CCODe:CODE
Secondary Serving Cell HS-SCCH 3 Chan
Code
GPIB command: CALL:SSCell:HSSCchannel3:CCODe:CODE
Secondary Serving Cell HS-SCCH 4 Chan
Code
GPIB command: CALL:SSCell:HSSCchannel4:CCODe:CODE
Number of Available HS-PDSCHs OVSF
Codes
This result returns the number of available OVSF codes for HS-PDSCHs.
Current
Service Type is not HSDPA/HSPA related (eg,
RB Test Mode - HSPA/HSDPA or PS
Data - HSPA/HSDPA
) in Active Cell Operating
Mode.Channel Type is not
12.2K+HSDPA , or 12.2K+HSPA , or HSPA
Only in FDD Test
Operationg Mode.Cell Off
or CW Operating Mode.GPIB command: CALL:STATus:HSPDschannel:AVAilable:COUNt?
The downlink
channel code preset (front panel: DL
Chan Code Preset Configs ) allows you to configure the
test set for 3GPP TS 34.121-1 channel code much easier (the DL
Channel Code Preset Configurations are only available from the
front panel; there are no GPIB commands to configure these presets).
The Operating
Mode must be set to Cell Off
before selecting one of the DL channel code preset configurations.
| 34.121 Table E.6.1.1(Non-HSDPA) | 34.121 Tables E.6.2.1,2(HSDPA 10 HS-PDSCHs) | 34.121 Tables E.6.2.3,4(HSDPA 15 HS-PDSCHs) | 34.121 Tables E.6.3.1,2(E-DCH 5 HS-PDSCHs) | |
|---|---|---|---|---|
| Shared DL Channel Codes | ||||
| 96 | 7 | 96 | ||
|
|
|
||
|
|
|
||
|
|
|
||
|
14 | 192 | ||
|
7 | 96 | ||
|
|
|
||
|
|
|
||
|
||||
|
2,3 | 2,3 | ||
2, 11, 17, 23, 31, 38, 47, 55, 62, 69, 78, 85, 94, 125, 113, 119 |
|
|
|
|
|
||||
|
||||
|
||||
|
|
|||
|
|
|||
|
|
|||
|
|
|||
| HSDPA RB Test Settings | ||||
|
||||
|
15 | 5 | ||
|
Compressed Mode with 384k DL DPCH(Non-HSDPA) |
|---|---|
| OCNS Codes | |
2, 11, 17, 23, 31, 38, 47, 55, 62, 69, 78, 85, 94, 92, 88, 90 |
|
The relative
level of all downlink channels can be individually set or turned
off (except that the P-CCPCH and the SCH are time multiplexed,
and use the same level for both channels). The level of each active
channel is a fraction of the Cell
Power (Îor) setting, expressed in dB. If the summed level
of all channels is less than one, the orthogonal coded noise source
(OCNS) is turned on to account for the difference (see Orthogonal Channel Noise Simulator (OCNS) ).
The downlink code channel levels currently in use (as well as the "desired" levels) are displayed in the Downlink Code Channel Information screen.
The downlink channel levels for idle mode (no DPCH is present) may be different than the levels used during a call (DPCH is present). Thus, there are two different level settings for the downlink channels in active cell operating mode: Downlink Channel Levels and Connected DL Channel Levels .
On must not be greater than 30 dB below the Total RF Power . Off
, the test set will not automatically
turn it back on if it is needed to perform a call processing
operation you've requested (for example, if you turn PICH Level to
Off , the Originate Call
procedure will fail). The Downlink Channel Levels set
of power levels is used when RRC State
is Idle or
CELL_FACH .
These levels
cannot be changed in the Active
Cell operating mode. You can query these settings via
GPIB and view them on the front panel during
Active Cell mode operation, but attempting to change
the levels during Active Cell
mode operation results in an error message (use the Cell Off operating mode to
change the active cell downlink channel levels).
CPICH
Level
GPIB command: CALL:CPIChannel
P-CCPCH/SCH Level
GPIB command: CALL:CCPChannel:PRIMary[:SLEVel]
S-CCPCH Level
GPIB command: CALL:CCPChannel:SECondary[:SLEVel]
PICH
Level
GPIB command: CALL[:CELL]:PICHannel[:SLEVel]
AICH
Level
GPIB command: CALL:AICHannel
DPCH Level
Note:
no DPCH is generated before the call is established. Setting DPCH
Level to a non-zero value simply adds that power
to the OCNS.
GPIB command: CALL:DPCHannel[:SLEVel]
The Connected DL Channel Levels
are used when RRC State is
CELL_DCH . These levels are applied after the RRC Connection
Setup message is sent by the test set during the RRC Connection Setup Procedure , directing
the UE to go into CELL_DCH (i.e.
once a DPCH has been established). When the DPCH channel is
released, the test set transitions back to the Downlink Channel Levels set.
These levels
can be changed in any operating mode, including
Active Cell . This allows you to vary the relative
channel levels while a call is connected in order to test
the UE's response.
These settings specify the connected downlink channel levels relative to Cell Power (Îor).
Cell 1 Connected CPICH Level
GPIB command: CALL:CONNected:CPIChannel[:SLEVel]
Cell 1 Connected P-CCPCH/SCH Level
GPIB command: CALL:CONNected:CCPChannel:PRIMary[:SLEVel]
Cell 1 Connected S-CCPCH Level
GPIB command: CALL:CONNected:CCPChannel:SECondary[:SLEVel]
Cell 1 Connected PICH Level
GPIB command: CALL:CONNected:PICHannel[:SLEVel]
Cell
1 Connected DPCH Level
Note: PO1, PO2 and PO3, which define the offset of the TFCI, TPC and pilot fields of the DPCCH relative to the DPDCH's power (see 3GPP TS 25.214 5.2.1.1) are always set to 0 in the test set (as specified by 3GPP TS 25.101 A.3 and 34.121 C.3).
GPIB command: CALL:CONNected:DPCHannel[:SLEVel]
Cell 2 CPICH Level ( lab application only , see Cell 2 Overview )Cell 2 P-CCPCH/SCH Level ( lab application only , see Cell 2 Overview )Cell 2 DPCH Level (
lab application only , see Cell
2 Overview )These settings are only applicable to the lab application or feature-licensed test application.
HSDPA Cell 1 Connected CPICH Level
GPIB command: CALL:CONNected:CPIChannel[:SLEVel]:HSDPa
HSDPA
Cell 1 Connected P-CCPCH/SCH Level
GPIB command: CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSDPa
HSDPA Cell 1 Connected S-CCPCH
Level
GPIB command: CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSDPa
HSDPA
Cell 1 Connected PICH Level
GPIB command: CALL:CONNected:PICHannel[:SLEVel]:HSDPa
HSDPA
Cell 1 Connected DPCH Level
Note: PO1, PO2 and PO3, which define the offset of the TFCI, TPC and pilot fields of the DPCCH relative to the DPDCH's power (see 3GPP TS 25.214 5.2.1.1) are always set to 0 in the test set (as specified by 3GPP TS 25.101 A.3 and 34.121 C.3).
GPIB command: CALL:CONNected:DPCHannel[:SLEVel]:HSDPa
HSDPA
Cell 1 Connected HS-PDSCHs Level (Sum)
This parameter sets the total amount of power in all HS-PDSCHs. The power is equally split between all HS-PDSCHs active during each subframe.
Note,
if you set this level to
Off , but do not turn HSDPA Cell
1 Connected HS-SCCH 1 Level Off
, the UE will NACK the packets assigned to it by HS-SCCH
1 (because the packets are not being sent to it on the
HS-PDSCHs, as their power level is off).
GPIB command: CALL:CONNected:HSPDschannel[:SLEVel]
HSDPA
Cell 1 Connected HS-SCCH 1 Level
Note,
if you set this level to
Off , the UE will not read the HS-PDSCHs for any
packets assigned to it. Depending upon the CQI Feedback Cycle (k) setting, the UE
may still transmit CQI data.
GPIB command: CALL:CONNected:HSSCchannel[1][:SLEVel]
HSDPA
Cell 1 Connected HS-SCCH 2 Level
GPIB command: CALL:CONNected:HSSCchannel2[:SLEVel]
HSDPA
Cell 1 Connected HS-SCCH 3 Level
GPIB command: CALL:CONNected:HSSCchannel3[:SLEVel]
HSDPA
Cell 1 Connected HS-SCCH 4 Level
GPIB command: CALL:CONNected:HSSCchannel4[:SLEVel]
HSDPA Cell 1 Antenna 2 Connected
P-CPICH Level
GPIB command: CALL:ANTenna2:CONNected:CPIChannel[:SLEVel]:HSDPa
HSDPA
Cell 1 Antenna 2 Connected S-CPICH Level
GPIB command: CALL:ANTenna2:CONNected:CPIChannel:SECondary[:SLEVel]:HSDPa
Secondary Cell HSDPA Conn CPICH
Level
GPIB command: CALL:SSCell:CONNected:CPIChannel:LEVel:HSDPa
Secondary Cell HSDPA Conn PCCPCH/SCH
Level
GPIB command: CALL:SSCell:CONNected:CCPChannel:PRIMary:LEVel:HSDPa
Secondary Cell HSDPA Conn PICH
Level
GPIB command: CALL:SSCell:CONNected:PICHannel:LEVel:HSDPa
Secondary Cell HSDPA Conn HSPDSCHs
Lvl (Sum)
GPIB command: CALL:SSCell:CONNected:HSPDschannel:LEVel:HSDPa
Secondary Cell HSDPA Conn HSSCCH
1 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel[1]:LEVel:HSDPa
Secondary Cell HSDPA Conn HSSCCH
2 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel2:LEVel:HSDPa
Secondary Cell HSDPA Conn HSSCCH
3 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel3:LEVel:HSDPa
Secondary Cell HSDPA Conn HSSCCH
4 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel4:LEVel:HSDPa
HSDPA
Antenna 2 Connected P-CPICH (Desired Level)
HSDPA
Antenna 2 Connected S-CPICH (Desired Level)
These settings are only applicable to the lab application or feature-licensed test application.
HSPA Cell 1 Connected CPICH Level
GPIB command: CALL:CONNected:CPIChannel[:SLEVel]:HSPA
HSPA
Cell 1 Connected P-CCPCH/SCH Level
GPIB command: CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSPA
HSPA Cell 1 Connected S-CCPCH Level
GPIB command: CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSPA
HSPA
Cell 1 Connected PICH Level
GPIB command: CALL:CONNected:PICHannel[:SLEVel]:HSPA
HSPA
Cell 1 Connected DPCH Level
Note: PO1, PO2 and PO3, which define the offset of the TFCI, TPC and pilot fields of the DPCCH relative to the DPDCH's power (see 3GPP TS 25.214 5.2.1.1) are always set to 0 in the test set (as specified by 3GPP TS 25.101 A.3 and 34.121 C.3).
GPIB command: CALL:CONNected:DPCHannel[:SLEVel]:HSPA
HSPA
Cell 1 Connected E-AGCH Level
GPIB command: CALL:CONNected:EAGChannel[:SLEVel]
HSPA
Cell 1 Connected E-HICH Level
The E-HICH and E-RGCH share the same channelization code (see E-HICH/E-RGCH Channelization Code ). The power in that channelization code is the sum of the HSPA Cell 1 Connected E-HICH Level and HSPA Cell 1 Connected E-RGCH Level.
GPIB command: CALL:CONNected:EHIChannel[:SLEVel]
HSPA
Cell 1 Connected E-RGCH Level
The E-HICH and E-RGCH share the same channelization code (see E-HICH/E-RGCH Channelization Code ). The power in that channelization code is the sum of the HSPA Cell 1 Connected E-HICH Level and HSPA Cell 1 Connected E-RGCH Level.
You must set RB Test Mode E-RGCH Information State to on in order for the UE to listen to the E-RGCH while on an HSPA RB Test Mode connection.
You must set PS Data E-RGCH Information State to on in order for the UE to listen to the E-RGCH while on an HSPA PS Data connection.
GPIB command: CALL:CONNected:ERGChannel[:SLEVel]
HSPA
Cell 1 Connected HS-PDSCHs Level (Sum)
This parameter sets the total amount of power in all HS-PDSCHs. The power is equally split between all HS-PDSCHs active during each subframe.
Note,
if you set this level to
Off , but do not turn HSPA
Cell 1 Connected HS-SCCH 1 Level Off
, the UE will NACK the packets assigned to it by HS-SCCH
1 (because the packets are not being sent to it on the
HS-PDSCHs, as their power level is off).
GPIB command: CALL:CONNected:HSPDschannel[:SLEVel]:HSPA
HSPA
Cell 1 Connected HS-SCCH 1 Level
Note,
if you set this level to
Off , the UE will not read the HS-PDSCHs for any
packets assigned to it. Depending upon the CQI Feedback Cycle (k) setting, the UE
may still transmit CQI data.
GPIB command: CALL:CONNected:HSSCchannel[1][:SLEVel]:HSPA
HSPA
Cell 1 Connected HS-SCCH 2 Level
GPIB command: CALL:CONNected:HSSCchannel2[:SLEVel]:HSPA
HSPA
Cell 1 Connected HS-SCCH 3 Level
GPIB command: CALL:CONNected:HSSCchannel3[:SLEVel]:HSPA
HSPA
Cell 1 Connected HS-SCCH 4 Level
GPIB command: CALL:CONNected:HSSCchannel4[:SLEVel]:HSPA
HSPA Cell 1 Antenna 2 Connected
P-CPICH Level
GPIB command: CALL:ANTenna2:CONNected:CPIChannel[:SLEVel]:HSPA
HSPA Cell 1 Antenna 2 Connected
S-CPICH Level
GPIB command: CALL:ANTenna2:CONNected:CPIChannel:SECondary[:SLEVel]:HSPA
Secondary Cell HSDPA Conn CPICH
Level
GPIB command: CALL:SSCell:CONNected:CPIChannel:LEVel:HSDPa
Secondary Cell HSPA Conn CPICH
Level
GPIB command: CALL:SSCell:CONNected:CPIChannel:LEVel:HSPA
Secondary Cell HSPA Cell 1 Connected
P-CCPCH/SCH Level
GPIB command: CALL:SSCell:CONNected:CCPChannel:PRIMary:LEVel:HSPA
Secondary Cell HSPA Conn PICH Level
GPIB command: CALL:SSCell:CONNected:PICHannel:LEVel:HSPA
Secondary Cell HSPA Conn HSPDSCHs
Levels (Sum)
GPIB command: CALL:SSCell:CONNected:HSPDschannel:LEVel:HSPA
Secondary Cell HSPA Conn HSSCCH
1 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel[1]:LEVel:HSPA
Secondary Cell HSPA Conn HSSCCH
2 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel2:LEVel:HSPA
Secondary Cell HSPA Conn HSSCCH
3 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel3:LEVel:HSPA
Secondary Cell HSPA Conn HSSCCH
4 Level
GPIB command: CALL:SSCell:CONNected:HSSCchannel4:LEVel:HSPA
HSPA
Antenna 2 Connected P-CPICH (Desired Level)
HSPA
Antenna 2 Connected S-CPICH (Desired Level)
These settings are only applicable to the lab application or feature-licensed test application.
Common
HS-DSCH CPICH Level
GPIB command: CALL[:CELL]:CHSDschannel:CPIChannel[:SLEVel]
Common
HS-DSCH P-CCPCH/SCH Level
GPIB command: CALL[:CELL]:CHSDschannel:CCPChannel:PRIMary[:SLEVel]
Common
HS-DSCH S-CCPCH Level
GPIB command: CALL[:CELL]:CHSDschannel:CCPChannel:SECondary[:SLEVel]
Common
HS-DSCH PICH Level
GPIB command: CALL[:CELL]:CHSDschannel:PICHannel[:SLEVel]
GPIB command: CALL[:CELL]:CHSDschannel:AICHannel[:SLEVel]
Common
HS-DSCH HS-PDSCHs Level(Sum)
GPIB command: CALL[:CELL]:CHSDschannel:HSPDschannel[:SLEVel]
Common HS-DSCH
HS-SCCH 1 Level
GPIB command: CALL[:CELL]:CHSDschannel:HSSCchannel[1][:SLEVel]
Common HS-DSCH
HS-SCCH 2|3|4 Level
GPIB command: CALL[:CELL]:CHSDschannel:HSSCchannel2|3|4[:SLEVel]
These settings are only applicable to the lab application or feature-licensed test application.
Common
E-DCH CPICH Level
GPIB command: CALL[:CELL]:CEDChannel:CPIChannel[:SLEVel]
Common
E-DCH P-CCPCH/SCH Level
GPIB command: CALL[:CELL]:CEDChannel:CCPChannel:PRIMary[:SLEVel]
Common
E-DCH S-CCPCH Level
GPIB command: CALL[:CELL]:CEDChannel:CCPChannel:SECondary[:SLEVel]
Common
E-DCH PICH Level
GPIB command: CALL[:CELL]:CEDChannel:PICHannel[:SLEVel]
GPIB command: CALL[:CELL]:CEDChannel:AICHannel[:SLEVel]
GPIB command: CALL[:CELL]:CEDChannel:FDPChannel[:SLEVel]
GPIB command: CALL[:CELL]:CEDChannel:EAGChannel[:SLEVel]
GPIB command: CALL[:CELL]:CEDChannel:EHIChannel[:SLEVel]
Common E-DCH
HS-PDSCHs Level(Sum)
GPIB command: CALL[:CELL]:CEDChannel:HSPDschannel[:SLEVel]
GPIB command: CALL[:CELL]:CEDChannel:HSSCchannel[1][:SLEVel]
Common E-DCH
HS-SCCH 2|3|4 Level
GPIB command: CALL[:CELL]:CEDChannel:HSSCchannel2|3|4[:SLEVel]
OCNS is used to simulate additional users on the downlink. OCNS is automatically enabled when the sum of the levels of all the enabled downlink physical channels is less than the cell power setting.
Cell 1 OCNS is made up of the following 16 separate code channels: 2, 11, 17, 23, 31, 38, 47, 55, 62, 69, 78, 85, 94, 113, 119, and 125, with an OVSF of 128. The fraction of the composite OCNS power that is allocated to each of the code channels making up the composite OCNS are as specified by 3GPP TS 34.121 sE.3.6.
Cell 2 OCNS ( lab application only ) consists of a single channel at OVSF 128,2.
As individual
downlink channel levels are adjusted, the composite OCNS level
is automatically set to a value equal to the difference between
the summed downlink channel levels and the cell power setting
(when the sum of the downlink code channel levels is such that
the composite OCNS is less than -30 dB, it is set to
Off ).
The OCNS currently in use (as well as the "desired" level) is displayed in the Downlink Code Channel Information window.
GPIB command: CALL:OCNSource (query only)
This section is only applicable to the lab application or feature-licensed test application.
When HSDPA or HSPA is active (see HSDPA Activation in FDD Test and HSDPA Activation in Active Cell ), the cell 1 OCNS is made up of the following 7 separate code channels: 122, 123, 124, 125, 126, and 127, with an OVSF of 128, rather than the code channels described in Orthogonal Channel Noise Simulator (OCNS) above. The fraction of the composite OCNS power that is allocated to each of the code channels making up the composite OCNS are as specified by 3GPP TS 34.121 sE.5.2.
The parameter
specifies whether S-CPICH is transmitted on antenna 2 when Current MIMO Configuration Status
is set to Active in Active Cell/FDD Test Operating Mode.
If Antenna 2 S-CPICH Configuration
is set to On , S-CPICH will
be transmitted on antenna 2 and its scrambling code will be Serving Cell Primary Scrambling Code
. If Antenna 2 S-CPICH Configuration
is set to Off , S-CPICH will
not be transmitted on antenna 2.
If you want to
change Ant2 S-CPICH Cfg to Off
, ensure that:
P-CPICH
Active
Cell/FDD Test Operating ModeOff.
You can change the setting via CALL:ANTenna2:CONNected:CPIChannel:SECondary:STATe:HSDPa
and CALL:ANTenna2:CONNected:CPIChannel:SECondary:STATe:HSPA
This setting
can only be set when the Call/Data
Status is Idle .
GPIB Command: CALL:ANTenna2:CPIChannel:SECondary:CONFig:STATe