Last updated: January 15, 2009
| Function |
Sets/queries the Mobile Network Code (MNC) for the currently selected application.
This setting can only be changed when call status is |
| 1 | |
| Requirements | |
OUTPUT 714;"CALL:CELL:MNCODE 10" !Sets the current MNC setting to 10. |
|
| Function |
Sets/queries the Mobile Network Code (MNC) , when using the W-CDMA application.
This setting can only be changed when call status is |
| 1 | |
| Requirements | |
OUTPUT 714;"CALL:CELL:MNCODE:WCDMA 10" !Sets the WCDMA mobile network code to 10. |
|