|
|
|
Last updated: October 30, 2013
|
Sets/queries the Authentication Key . This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF |
|
|
Range: "00000000:00000000:00000000:00000000" to FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate '4147494C454E5420544543484E4F0000'" ! Sets the authentication key to 4147494C:454E5420:54454348:4E4F0000. |
|
|
Sets/queries the Authentication Algorithm . This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:ALGorithm RIJN" !Sets the authentication algorithm to Milenage (Rijndael). |
|
|
Sets/queries the AMF Value . This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFF |
|
|
Range: "0000" to "FFFF" |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:AMF 'FFFF'" !Sets the AMF value to FFFF. |
|
|
Sets/queries the Operator Variant Parm Type . You must then enter a value for Operator Variant Auth Alg (CALL:SECurity:AUTHenticate:OPVariant:PVALue ). This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:OPVariant:PTYPe OP" !Sets the Operator Variant Authentication Parameter type to OP. |
|
|
Sets/queries the value of the Operator Variant Auth Alg . You must indicate, using the Operator Variant Parm Type setting (CALL:SECurity:AUTHenticate:OPVariant:PTYPe ), whether this setting contains OP or OPc. This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF |
|
|
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:OPVariant:PVALue '10F'" ! Sets the value of Operator Variant Authentication ! Parameter to 00000000:00000000:00000000:0000010F. |
|
|
Sets/queries the Random (RAND) Value . This setting is not useful until the security operation mode is set to other than "NONE". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF |
|
|
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:RANDom 'A'" !Sets the random value of the Authentication Parameter to 00000000:00000000:00000000:0000000A. |
|
|
Queries the Authentication Result: GMM . |
|
|
Range: SUCCess|MSFAILMAC|MSFAILSYNC|MSFAILUNKNOWN|RESLENERR|
|
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:RESult:GMM?" !Queries the GMM authentication result. |
|
|
Queries the Authentication Result: MM . |
|
|
Range: SUCCess|MSFAILMAC|MSFAILSYNC|MSFAILUNKNOWN|RESLENERR|
|
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:RESult?" !Queries the MM authentication result. |
|
|
Resets the authentication sequence number (SQN) to zero (see Reset Authentication SQN ). |
|
| Requirements | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:SQN:RESet" !Resets the authentication SQN. |
|
|
Sets/queries IMEISV Request State . |
|
| Same as setting. | |
| 0 (OFF) | |
| Requirements | Lab Application Revision: J.00.00 and above |
OUTPUT 714;"CALL:SECurity:EISV:REQuest ON" !Requests the UE to report its IMEISV value via authentication and ciphering response message. |
|
|
Sets/queries Security Operations . |
|
| Requirements |
Test Application Revision: A.03 and above. |
OUTPUT 714;"CALL:SECurity:OPERation AUTHONLY" !Sets the security procedure with authentication only. |
|
|
Queries the Integrity Key . This result is only applicable for the security operation mode of "Authentication and Integrity Protection" or "Authentication, Integrity Protection and Ciphering". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF |
|
|
Range: "00000000:00000000:00000000:00000000" to FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF |
|
| Requirements |
Test Application Revision: A.17.00 and above. |
OUTPUT 714;"CALL:SECurity:RESult:INTegrity:key?" ! Query the integrity key. |
|
|
Queries the Ciphering Key . This result is only applicable for the security operation mode of "Authentication, Integrity Protection and Ciphering". See CALL:SECurity:OPERation . |
|
|
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF |
|
|
Range: "00000000:00000000:00000000:00000000" to FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF |
|
| Requirements |
Test Application Revision: A.17.00 and above. |
OUTPUT 714;"CALL:SECurity:RESult:CIPHering:key?" ! Sets the ciphering key. |
|
|
|
|