Last updated: January 16, 2009
|
Sets/queries the downlink dedicated physical channel's (DPCH) channelization code during the "setup" phase of connection setup when CALL[:CELL]:SRBearer:CCHannel:DEDicated:DRATe[:MANual] is set to BPS3400 or BPS2200. When CALL[:CELL]:SRBearer:CCHannel:DEDicated:DRATe[:MANual] is set to BPS13600, the DPCH channelization code will be determined by the UTRA FDD DL DPCH 12.2 RMC channelization code ( CALL:DPCHannel:RMC12:CCODe ). See Signalling Radio Bearer (SRB) Parameters . This setting cannot be changed while the active cell operating mode. Attempting to change this setting while in this mode will result in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode to change this setting. To set the DPCH channelization code for the SRB when using the Lab Application, see CALL:DPCHannel:KSPS15[:CCODe] and CALL:DPCHannel:KSPS30[:CCODe] . |
|
|
CODE12|CODE13CODE20|CODE21|CODE40|CODE43|CODE58|CODE126|CODE127| |
|
| Same as setting | |
OUTPUT 714;"CALL:CELL:SRBearer:CCHannel:DEDicated:BPS3400:CCODE CODE58" |
|
|
Sets/queries Manual SRB Configuration .
This setting is only applicable when
CALL[:CELL]:SRBearer:CCHannel:DEDicated:DRATe:CONTrol:AUTO
is set to This setting cannot be changed in Active Cell Operating Mode. |
|
|
Test or Lab Application Revision: A.01 and above. Test Application Revision A.03 added BPS2200 setting. Test Application Revision A.10.01 and Lab Application Revision D.01.01 added [:MANual] |
|
OUTPUT 714;"CALL:CELL:SRBEARER:CCHANNEL:DEDICATED:DRATE BPS13600" ! Sets Manual SRB Configuration to 13.6K DCCH. |
|
|
Sets/queries
SRB Configuration Control
. When set to This setting cannot be changed in Active Cell Operating Mode. |
|
OUTPUT 714;"CALL:SRBearer:CCHannel:DEDicated:DRATe:CONTrol:AUTO ON" ! Sets SRB Configuration Control to Auto. |
|