Last updated: January 16, 2009
|
Queries the desired total RF power for the current system type. Total RF Power is a calculated value, that is the sum of cell power and AWGN power settings. (See Cell Power, AWGN Power and Total RF Power Ranges for more information about desired versus current power levels.) |
|
| -75 dBm/3.84 MHz | |
OUTPUT 714;"CALL:TOTAL:POWER:AMPLITUDE?" |
|
|
Queries the total RF power state for the current system type. The total RF power state is 1 (on) if either cell power or AWGN power is on. The return value for this query is not necessarily the total power state at the moment this command is processed by the test set. To query the power state of the test set at the moment, use the CALL:STATus:TOTal:POWer:STATe? command. |
|
| 1 (on) | |
OUTPUT 714;"CALL:TOTAL:POWER:STATE?" |
|