Last updated: January 16, 2009
|
Turns on/off the auto Measurement Frequency feature which determines the measurement downconverter signal path frequency control mode. (See Block Diagram .) OFF = manual (see RFANalyzer:MANual:MEASurement[:MFRequency] and RFANalyzer:MANual:MEASurement:FREQuency )
Note, when you switch between operating modes, |
|
| Range: 1|ON|0|OFF | |
| *RST setting | 1 (on) |
OUTPUT 714;"RFANalyzer:CONTrol:MEASurement:FREQuency:AUTO OFF" !Enables manual control of the measurement signal path tune frequency. |
|
|
Sets/queries Power Control . OFF = manual (see RFANalyzer:MANual:POWer[:SELected] )
This command is available in
Note, when you switch between operating modes, |
|
| *RST setting | 1 (on) |
OUTPUT 714;"RFANALYZER:CONTROL:POWER:AUTO OFF" !Enables manual control of the expected input power level. |
|
|
Turns on/off the auto Uplink Frequency feature, which determines the test set's demodulation signal path tune frequency control mode. OFF = manual (see RFANalyzer:MANual:UPLink[:MFRequency] and RFANalyzer:MANual:UPLink:FREQuency . This setting is available in FDD Test and CW operating modes.
Note, when you switch between operating modes, |
|
| *RST setting | 1 (on) |
OUTPUT 714;"RFANALYZER:CONTROL:UPLINK:FREQUENCY:AUTO OFF" !Enables manual control of the demodulation signal path tune frequency. |
|
|
Sets/queries the expected CW receiver input power. This setting is only used when the Operating Mode is set to CW. (See CALL:OPERating .) |
|
| *RST setting | +13 dBm |
OUTPUT 714;"RFANALYZER:CW:EXPECTED:POWER -20" |
|
|
Sets/queries
Manual Power
(the optional [:SELected] keyword in this command specifies that the manual power setting applies to the current system type). This command is only applicable when
RFANalyzer:CONTrol:POWer:AUTO
(
This command is available in
Note, when you switch between operating modes, |
|
|
Range: Test application and system type dependent (approximately -25 to +43 dBm). |
|
| Range: Test application and system type dependent (approximately -25 to +43 dBm). | |
| *RST setting | -75 dBm |
OUTPUT 714;"RFANALYZER:MANUAL:POWER:SELECTED 24 DBM" !Sets the manual power control mode expected input power level for the currently selected system type to 24 dBm. |
|
|
Sets/queries
Manual Power
when UTRA FDD is the current system type. This command is only applicable when
RFANalyzer:CONTrol:POWer:AUTO
(
This command is available in
Note, when you switch between operating modes, |
|
|
Range: -129 to +80 dBm (-79 dBm to +30 dBm actual hardware range with amplitude offset = 0) |
|
| Range: -129 to +80 dBm (-79 dBm to +30 dBm actual hardware range with amplitude offset = 0) | |
| *RST setting | 0 dBm |
OUTPUT 714;"RFANALYZER:MANUAL:POWER:FDD 24 DBM" !Sets the manual power control mode expected input power level for the FDD system type to !24 dBm. |
|
|
The setting form of this command performs two functions: (1) sets Measurement Frequency , the tune frequency of the test set's measurement signal path, and (2) selects manual (auto off) tune mode for the test set's measurement signal path. The query form of this command returns the tune frequency of the test set's measurement signal path. The tune mode for the test set's measurement signal path can be returned to auto using the RFANalyzer:CONTrol:MEASurement:FREQuency:AUTO command.
Note, when you switch between operating modes, |
|
| Range: 292.5 MHz to 2700 MHz | |
| *RST setting | 896 MHz |
OUTPUT 714;"RFANALYZER:MANUAL:MEASUREMENT:MFREQUENCY 942.6 MHZ" !Enables manual control of the measurement signal path tune frequency and sets the tune frequency to 942.6 MHz. |
|
|
Sets/queries Measurement Frequency .
This setting is applied when manual mode is selected for
Note, when you switch between operating modes, |
|
| Range: 292.5 MHz to 2700 MHz | |
| *RST setting | 896 MHz |
OUTPUT 714;"RFANALYZER:MANUAL:MEASUREMENT:FREQUENCY 942.6 MHZ" !Sets the measurement signal path tune frequency to 942.6 MHz when manual control mode is used. |
|
|
The setting form of this command performs two functions: (1) sets Uplink Frequency , the tune frequency of the test set's demodulation signal path, and (2) selects manual (auto off) tune mode for the test set's demodulation signal path. The query form of this command returns the tune frequency of the test set's demodulation signal path. The tune mode for the test set's demodulation path can be returned to auto using the RFANalyzer:CONTrol:UPLink:FREQuency:AUTO command. This setting is available in FDD Test and CW operating modes.
Note, when you switch between operating modes, |
|
| Range: 292.5 MHz to 2700 MHz | |
| *RST setting | 896 MHz |
OUTPUT 714;"RFANALYZER:MANUAL:UPLINK:MFREQUENCY 1955.030 MHZ" !Enables manual control of the demodulation signal path tune frequency and sets the tune frequency !to 1955.030 MHz. |
|
|
Sets/queries Uplink Frequency .
This setting is applied when manual mode is selected for This setting is available in FDD Test and CW operating modes.
Note, when you switch between operating modes, |
|
| *RST setting | 896 MHz |
OUTPUT 714;"RFANALYZER:MANUAL:UPLINK:FREQUENCY 942.6 MHZ" !Sets the test set's demodulation signal path tune frequency to 942.6 MHz. |
|