This section is only applicable to the lab application or feature-licensed test application.
Sets/queries the Number of Frequency Steps . |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:FREQuency:STEP:COUNt 10" !Sets the number of frequency steps to 10. |
|
Sets/queries the MS RX Frequency Step Values . If you set fewer than 40 values, the remaining values are set to NAN (9.91E+37). |
|
|
Although you can enter any frequencies between 421 and 2170 MHz, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only test frequencies within a single W-CDMA/HSDPA frequency band range: |
|
| Same as setting | |
1933.0MHz, 1933.2MHz, 1933.4MHz, 1933.6MHz, 1933.8MHz, 1934.0MHz, 1934.2MHz, 1934.4MHz, 1934.6MHz, 1934.8MHz, 1935.0MHz, 1935.2MHz, 1935.4MHz, 1935.6MHz, 1935.8MHz, 1936.0MHz, 1936.2MHz, 1936.4MHz, 1936.6MHz, 1936.8MHz, 872.0MHz, 872.2MHz, 872.4MHz, 872.6MHz, 872.8MHz, 873.0MHz, 873.2MHz, 873.4MHz, 873.6MHz, 873.8MHz, 874.0MHz, 874.2MHz, 874.4MHz, 874.6MHz, 874.8MHz, 875.0MHz, 875.2MHz, 875.4MHz, 875.4MHz, 875.6MHz, 875.8MHz |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 or D.00.04 and above. Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2622.4 to 2687.6 MHz (Band VII) Test Application Revision A.21 and above: Extends the frequency band range. |
|
OUTPUT 714;"SETup:CFDTune:MS:RX:FREQuency:STEP 1932.4 MHz, 1937.4 MHz, 1942.4 MHz, 1947.4 MHz, 1952.4 MHz" ! Sets MS RX Frequency Step Values to 1932.4 MHz, 1937.4 MHz, 1942.4 MHz, 1947.4 MHz, ! 1952.4 MHz, followed by 35 NANs (9.91E+37) |
|
| Sets/queries the MS RX Frequency Step Start Index . | |
| Same as setting | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:MS:RX:FREQuency:STEP:STARt 6" !Sets the MS RX Frequency Step Start Index to 6. |
|
Sets/queries the MS RX Power Step Levels . If you set fewer than 40 values, the remaining values are set to NAN (9.91E+37). |
|
|
Although you can enter any power levels between -165 and 37 dBm, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, the test set can only transmit test power levels in the range of -115 to -13 dBm ( RF IN/OUT ) or -115 to -5 dBm ( RF OUT ONLY ). These ranges assume an amplitude offset of 0; the allowable ranges change as you change amplitude offsets, see Cell Power, AWGN Power and Total RF Power Ranges . |
|
| Same as setting | |
| -15.0dBm, -20.0dBm, -25.0dBm, -30.0dBm, -35.0dBm, -40.0dBm, -45.0dBm, -50.0dBm, -55.0dBm, -60.0dBm, -65.0dBm, -70.0dBm, -75.0dBm, -80.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm, -85.0dBm | |
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 or D.00.04 and above. Test Application Revision A.10 and Lab Application D.01, added support for RF OUT ONLY port. |
|
OUTPUT 714;"SETup:CFDTune:MS:RX:POWer:STEP -16, -20, -30, -40, -50,-60, -70, -80, -90, -100" ! Sets MS RX Power Step Levels to -16, -20, -30, -40, -50,-60, -70, -80, -90, -100 dBm, ! followed by 30 NANs (9.91E+37). |
|
| Sets/queries the MS RX Power Step Start Index . | |
| Same as setting | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:MS:RX:POWer:STEP:STARt 6" !Sets the MS RX Power Step Start Index to 6. |
|
Sets/queries the MS TX Frequency Step Values . If you set fewer than 40 values, the remaining values are set to NAN (9.91E+37). |
|
|
Although you can enter any frequencies between 411 and 1980 MHz, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only test frequencies within a single W-CDMA/HSDPA frequency band range: |
|
| Same as setting | |
1853.0MHz,
1853.2MHz, 1853.4MHz, 1853.6MHz, 1853.8MHz, 1854.0MHz, 1854.2MHz,
1854.4MHz, 1854.6MHz, 1854.8MHz, 1855.0MHz, 1855.2MHz, 1855.4MHz,
1855.6MHz, 1855.8MHz, 1856.0MHz, 1856.2MHz, 1856.4MHz, 1856.6MHz,
1856.8MHz, 827.0MHz, 827.2MHz, 827.4MHz, 827.6MHz, 827.8MHz,
828.0MHz, 828.2MHz, 828.4MHz, 828.6MHz, 828.8MHz, 829.0MHz,
829.2MHz, 829.4MHz, 829.6MHz, 829.8MHz, 830.0MHz, 830.2MHz,
830.4MHz, 830.6MHz, 830.8MHz, |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 or D.00.04 and above. Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2502.4 to 2567.6 MHz (Band VII) Test Application Revision A.21 and above: Extends the frequency band range. |
|
OUTPUT 714;"SETup:CFDTune:MS:TX:FREQuency:STEP 882.4 MHz, 893.4 MHz, 898.4 MHz, 903.4 MHz, 908.4 MHz" ! Sets MS TX Frequency Step Values to 882.4 MHz, 893.4 MHz, 898.4 MHz, 903.4 MHz, 908.4 MHz, followed by 35 NANs (9.91E+37) |
|
| Sets/queries the MS TX Frequency Step Start Index . | |
| Same as setting | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:MS:TX:FREQuency:STEP:STARt 6" !Sets the MS TX Frequency Step Start Index to 6. |
|
Sets/queries the MS TX Power Step Levels . If you set fewer than 40 values, the remaining values are set to NAN (9.91E+37). |
|
|
Although you can enter any power levels between -129 and +80 dBm (because this measurement is common to the W-CDMA/HSDPA, 1xEV-DO and cdma2000 formats), when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only measure power levels in the range of -70 to +30 dBm and the measurement is only specified for power levels in the range of -61 to +28 dBm (these ranges assume an amplitude offset of 0; the ranges change as you change amplitude offsets, see Amplitude Offset ). |
|
| Same as setting | |
| 12.0dBm, 7.0dBm, 2.0dBm, -8.0dBm, -13.0dBm, -18.0dBm, -23.0dBm, -28.0dBm, -33.0dBm, -38.0dBm, -43.0dBm, -48.0dBm, -53.0dBm, -58.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm, -63.0dBm | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:MS:TX:POWer:STEP 20, 16, 12, 8, 4, 0, -4, -8, -12, -16, -20, -30, -40, -50" ! Sets Rx Power Step Levels to 20, 16, 12, 8, 4, 0, -4, -8, -12, -16, -20, -30, -40, -50, ! followed by 26 NANs (9.91E+37). |
|
| Sets/queries the MS TX Power Step Start Index . | |
| Same as setting | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:MS:TX:POWer:STEP:STARt 6" !Sets the MS TX Power Step Start Index to 6. |
|
Sets/queries the Number of Power Steps . |
|
Test
Application Revision: A.09 and above, with the required feature
license |
|
OUTPUT 714;"SETup:CFDTune:POWer:STEP:COUNt 15" !Sets the number of power steps to 15. |
|
Test Application Revision: A.13 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:POWer:STEP:LENGth MS20" !Sets the power step length to 20 ms. |
|
The setting form of this command performs two functions: (1) sets the Fast Device Tune measurement's timeout (see Measurement Timeouts ) value, and (2) sets the Fast Device Tune measurement's timeout state to 1 (on). The query form returns the Fast Device Tune measurement's timeout value. |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:TIMeout 5S" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
| Sets/queries Fast Device Tune measurement's timeout state (see Measurement Timeouts ). | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:TIMeout:STATe ON" |
|
| Sets/queries Fast Device Tune measurement's timeout (see Measurement Timeouts ) setting to be used when the timeout state is set to ON. | |
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:CFDTune:TIMeout:TIME 5S" |
|