This section is only applicable to the lab application or feature-licensed test application.
Last updated: October 30, 2014
The Fast Device Tune measurement allows you to simultaneously calibrate your mobile station's transmitter (TX) output power and receiver (RX) input level across level and frequency in a single sweep (per frequency band range). The measurement is not performed with a call established between the test set and mobile station (MS). Rather, you must place your MS into a test mode which forces it to transmit a predefined series of power steps at various frequencies, and forces it to simultaneously tune its receiver to perform measurements of the test set's signal (to determine CPICH RSCP, for example) at various frequencies and power levels.
Before initiating the measurement, you must specify the power sequence that the MS will transmit (MS TX Power Sequence), and the frequencies at which the MS will transmit the power sequence (MS TX Frequency Sequence). You must also specify the power sequence you want the test set to transmit (MS RX Power Sequence), and the frequencies at which you want the test set to transmit the power sequence (MS RX Frequency Sequence).
The MS TX Power Sequence may include up to 40 steps (of 10 ms or 20 ms duration) that span some or all of the measurement's input range (the levels can step up or down with varying magnitudes of change, as long as the first step in the sequence provides a 20 dB rise to trigger the measurement). The MS TX Frequency Sequence may include up to 20 frequencies (within one frequency band range).
The test set can measure a total of 400 power points in one measurement cycle (for example: 20 power values at 20 different frequencies). However, the measurement allows you to enter up to 40 MS TX Power Step Levels and 40 MS TX Frequency Step Values (indexed from 0 to 39). You must then use the MS TX Power Step Start Index and Number of Power Steps settings to specify which power steps comprise the MS TX Power Sequence, and the MS TX Frequency Step Start Index and Number of Frequency Steps settings to specify which frequency steps comprise the MS TX Frequency Sequence. See Frequency/Power Series Example for an example illustrating how to utilize this flexibility.
The test set uses the values in the MS TX Power Sequence and the MS TX Frequency Sequence to build the MS TX Frequency/Power Series, which drives how the test set's receiver is tuned throughout the measurement cycle. To build the MS TX Frequency/Power Series, the test set simply repeats the MS TX Power Sequence at each of the frequencies in the MS TX Frequency Sequence, and inserts a frequency re-tune step in between each repetition of the power sequence (to allow the test set and MS to re-tune to the new frequency; no measurements are performed by the test set during the frequency re-tune steps). During the frequency re-tune steps, the test set tunes its receiver to the power and frequency values required for the first step in the next power sequence. The frequency re-tune steps are the same step length as the power sequence steps (10ms or 20 ms).
Before initiating the measurement, you must ensure that your MS is set to transmit the MS TX Frequency/Power Series you've set in the test set, including the frequency re-tune steps.
While the test set is measuring the MS TX Power Sequence, it also transmits a MS RX Power Sequence for the MS to measure. This MS RX Power Sequence must include the same number of power steps as the MS TX Power Sequence (up to 40 steps of 10 ms or 20 ms duration). These steps can be at any power level in the test set's Cell Power output range.
The test set transmits its MS RX Power Sequence at each of the frequencies in the MS RX Frequency Sequence. The MS RX Frequency Sequence may include up to 20 frequencies within one frequency band range (which does not have to be the same frequency band range as the MS TX Frequency Sequence). The number of frequencies in the MS RX Frequency Sequence must match the number of frequency steps in the MS TX Frequency Sequence.
If you do not want the MS to measure test set power at as many power levels or frequencies as you want the test set to measure from the MS, simply place "dummy" power levels or frequencies at the end of the MS RX Power Sequence and MS RX Frequency Sequence (for example, simply repeat the final power level or frequency). You can then ignore the mobile station's measurement results for these "dummy" points. Likewise, if you need more measurement points in the MS RX Frequency/Power Series than in the MS TX Frequency/Power Series, you can place "dummy" power levels and frequencies in the MS TX Frequency/Power Series, but note that the test set will still measure and report power for these "dummy" points. You must simply ignore these results.
As with the MS TX Frequency/Power Series, the test set can transmit a total of 400 power points in one measurement cycle (for example: 20 power values at 20 different frequencies), but the measurement allows you to enter up to 40 MS RX Power Step Levels and 40 MS RX Frequency Step Values (indexed from 0 to 39). You must then use the MS RX Power Step Start Index and Number of Power Steps settings to specify which power steps comprise the MS RX Power Sequence, and the MS RX Frequency Step Start Index and Number of Frequency Steps settings to specify which frequency steps comprise the MS RX Frequency Sequence. See Frequency/Power Series Example for an example illustrating how to utilize this flexibility.
As with the MS TX Frequency/Power Series, the test set uses the values in the MS RX Power Sequence and the MS RX Frequency Sequence to build the MS RX Frequency/Power Series, which drives how the test set's generator is tuned throughout the measurement cycle. To build the MS RX Frequency/Power Series, the test set simply repeats the MS RX Power Sequence at each of the frequencies in the MS RX Frequency Sequence, and inserts a frequency re-tune step in between each repetition of the power sequence (to allow the test set and MS to re-tune to the new frequency; the MS should not perform any measurements on the test set's signal during this time, or if a measurement is performed, you should ignore the measurement results). During the frequency re-tune steps, the test set moves its generator to the power and frequency values required for the first step in the next power sequence. The frequency re-tune steps are the same step length as the power sequence steps (10ms or 20 ms).
Before initiating the measurement, you must ensure that your MS is set to measure the MS RX Frequency/Power Series you've set in the test set, and that its tuning profile includes the frequency re-tune steps. Your mobile station should be configured to measure the test set's signal 5 ms after the start of each step, to allow the test set's source to settle.
To configure the downlink code channels transmitted by the test set during the MS RX Frequency/Power Series, see Downlink Channel Codes and Levels .
The test set can measure/transmit 400 power points in one measurement cycle. However, you can enter up to 40 power values and 40 frequencies for both the MS TX and MS RX sequences. This flexibility is present to make it more efficient for you to test different power sequences over different sets of frequencies or, more commonly, to test the same power sequence over different bands. You must load in the superset of power levels and frequency values once. Then for each measurement cycle, you simply change the start index and number of steps as needed and initiate the measurement.
For example, to measure a MS TX sequence of 14 power step levels in both the US Cellular and US PCS frequency bands:
and to transmit a MS RX sequence of 8 power step levels for the mobile station to measure:
for multiple US Cellular/US PCS mobile stations, set the following:
MS TX Power 
			 Step Levels = 20, 16, 12, 8, 4, 0,-4, -8, -12, -16, 
			 -20, -30, -40, -50MS RX Power Step Levels 
			 = -90, -80, -70, -60, -50, -40, -30, -20, -75, -75, -75, -75, 
			 -75, -75 (note that the last six values are "dummy" 
			 values required so that there are an equal number of power 
			 steps in the MS TX and MS RX sequences)MS TX Frequency Step Values 
			 = 826.4, 830.4, 834.4, 838.4, 842.4, 846.4, 1852.4, 1856.4, 
			 1860.4, 1864.4, 1870.4, 1874.4, 1878.4, 1882.4, 1886.4, 1890.4, 
			 1894.4, 1898.4, 1902.4MS RX Frequency Step Values 
			 = 871.4, 875.4, 879.4, 883.4, 887.4, 891.4, 1932.4, 1936.4, 
			 1940.1, 1944.4, 1950.4, 1954.4, 1958.4, 1962.4, 1966.4, 1970.4, 
			 1974.4, 1978.4, 1982.4MS 
			 TX Power Step Start Index = 0MS RX Power Step Start Index 
			 = 0Number of Power Steps = 
			 14MS TX 
				 Frequency Step Start Index = 0MS RX Frequency Step Start 
				 Index = 0Number of Frequency Steps 
				 = 6MS TX Frequency Step Start Index 
				 = 6MS RX Frequency Step Start 
				 Index = 6Number of Frequency Steps 
				 = 13The MS must trigger the measurement with a positive change in power of at least 20 dB (the mobile station's power must rise from 20 dB below the level of the first step in the MS TX Power Sequence to within 9 dB of the level of the first step).
To ensure successful triggering, it is recommended that you do the following:
1 
			 , indicating that the measurement is armed and ready to be 
			 triggered (or wait ~2 seconds if running the measurement from 
			 the front panel).Once triggered, the Fast Device Tune measurement performs a series of channel power measurements, one near the center of each step of the MS TX Power Sequence (while simultaneously transmitting the MS RX Power Sequence you've specified), then repeats the measurements at the next specified MS TX frequency (while simultaneously transmitting the MS RX Power Sequence at the next specified MS RX frequency). The test set tunes its receiver for each step according to the power levels you've specified for the MS TX Power Sequence. The MS must step its power according to the MS TX Power Sequence (and be within +/- 9 dB of the expected power level for each step) and hold its power constant for the duration of the measurement interval (666.7 us, 6.3 ms after the start of each 20 ms step, or 3.15 ms after the start of each 10 ms step.). After completing a measurement at each step of the MS TX Frequency/Power Series, the measurement returns power results for all of the measured steps.
Operating 
			 Mode must be set to FDD 
			 Test .Channel 
			 Type must be set to one of the Symmetrical 
			 RMCs (Note, this measurement is not supported on HSDPA 
			 or HSPA connections.)Manual 
			 .Measurement Frequency 
			 to manual control from the front panel, press the OFF/MANUAL 
			 key. This sets Measurement Frequency 
			 to the last frequency value that this parameter was set to. 
			 The Fast Device Tune measurement ignores the specific value 
			 that Measurement Frequency 
			 is set to, so it can be set to any supported input frequency; 
			 the measurement simply requires that Measurement 
			 Frequency be in manual control mode.Manual 
			 .Off 
			 . The Fast Device Tune 
		 measurement must re-range and re-trigger for every step in the 
		 MS TX Power Sequence. To ensure that this process is not interrupted 
		 by other operations, it is recommended that you not send any GPIB 
		 commands to the test set or press any front panel keys until the 
		 measurement has completed. If the measurement misses a trigger, 
		 it aborts and returns Integrity Indicator 
		 30 : Missed 
		 Trigger .
No other measurements can be running when a Fast Device Tune measurement is performed. If any measurements are running when a Fast Device Tune measurement is initiated, they are closed and a message is displayed to indicate that they were closed. Likewise, if any other measurements are initiated while a Fast Device Tune measurement is running, the Fast Device Tune measurement is closed and a message is displayed.
 Measurement results 
		 (and the RF generator output level) are affected by any RF IN/OUT Amplitude Offsets that 
		 are entered (see Amplitude 
		 Offset ).
 See Measurement Timeouts . Ensure that you set 
			 the Measurement Timeout 
			 to a value great enough to allow you to command the MS to 
			 transmit its MS TX Frequency/Power Series and for the test 
			 set to measure the MS TX Frequency/Power Series. For example, 
			 measuring the maximum allowable number of 400 power points 
			 can take more than 10 seconds (400 steps plus the 19 re-tune 
			 steps: 419 x 20 ms = 8.4 seconds, plus ~ 2 seconds required 
			 for the measurement to prepare for triggering).
GPIB command: SETup:CFDTune:TIMeout[:STIMe]
Indicates the step length that the test sets expects for each MS Tx/Rx power step. You can use either 20 ms or 10 ms step length.
GPIB command: SETup:CFDTune:POWer:STEP:LENGth
Indicates which of the MS TX Power Step Levels is the first step in the MS TX Power Sequence.
 This parameter 
			 can be set to any integer value between 0 and 39. However, 
			 MS TX Power Step Start Index 
			 + Number 
			 of Power Steps must not exceed 40.
 Also, you must 
			 ensure that the range of values selected by MS 
			 TX Power Step Start Index and Number 
			 of Power Steps do not include any NANs (9.91E+37) or 
			 values that are outside of the input range for the current 
			 application format (considering the amplitude offset settings).
GPIB command: SETup:CFDTune:MS:TX:POWer:STEP:STARt:[INDex]
Indicates which of the MS TX Frequency Step Values is the first frequency in the MS TX Frequency Sequence.
 This parameter 
			 can be set to any integer value between 0 and 39. However, 
			 MS TX Frequency Step Start Index 
			 + Number 
			 of Frequency Steps must not exceed 40.
 Also, the frequencies 
			 indicated by MS TX Frequency 
			 Step Start Index and Number 
			 of Frequency Steps must be within one frequency band 
			 range (and must not include any NANs (9.91E+37)).
GPIB command: SETup:CFDTune:MS:TX:FREQuency:STEP:STARt:[INDex]
Indicates which of the MS RX Power Step Levels is the first step in the MS RX Power Sequence.
 This parameter 
			 can be set to any integer value between 0 and 39. However, 
			 MS RX Power Step Start Index 
			 + Number 
			 of Power Steps must not exceed 40.
 Also, you must 
			 ensure that the range of values selected by MS 
			 RX Power Step Start Index and Number 
			 of Power Steps do not include any NANs (9.91E+37) or 
			 values that are outside of the output range for the current 
			 application format (considering the amplitude offset settings).
GPIB command: SETup:CFDTune:MS:RX:POWer:STEP:STARt:[INDex]
Indicates which of the MS RX Frequency Step Values is the first frequency in the MS RX Frequency Sequence.
 This parameter 
			 can be set to any integer value between 0 and 39. However, 
			 MS RX Frequency Step Start Index 
			 + Number 
			 of Frequency Steps must not exceed 40.
 Also, the frequencies 
			 indicated by MS RX Frequency 
			 Step Start Index and Number 
			 of Frequency Steps must be within one frequency band 
			 range (and must not include any NANs (9.91E+37)).
GPIB command: SETup:CFDTune:MS:RX:FREQuency:STEP:STARt:[INDex]
Indicates how many (consecutive) MS TX Power Step Levels are used for the MS TX Power Sequence, and how many (consecutive) MS RX Power Step Levels are used for the MS RX Power Sequence.
 This parameter 
			 can be set to any integer value between 1 and 40, but MS TX Power Step Start Index + Number 
			 of Power Steps and MS RX Power Step 
			 Start Index + Number of Power 
			 Steps must not exceed 40.
 Also, you must 
			 ensure that the range of power values selected by MS 
			 TX Power Step Start Index,  and MS 
			 RX Power Step Start IndexNumber 
			 of Power Steps do not include any NANs (9.91E+37) or 
			 values that are outside of the input or output ranges for 
			 the current application format (considering the amplitude 
			 offset settings).
GPIB command: SETup:CFDTune:POWer:STEP:COUNt
Indicates how many (consecutive) MS TX Frequency Step Values are used for the MS TX Frequency Sequence, and how many (consecutive) MS RX Frequency Step Values are used for the MS RX Frequency Sequence.
 This parameter 
			 can be set to any integer value between 1 and 20, but MS TX Frequency Step Start Index + Number of Frequency Steps and 
			 MS 
			 RX Frequency Step Start Index + Number 
			 of Frequency Steps must not exceed 40.
 Note that the 
			 frequencies indicated by MS TX 
			 Frequency Step Start Index and Number 
			 of Frequency Steps must be within one frequency band 
			 range. Likewise, the frequencies indicated by MS 
			 RX Frequency Step Start Index and Number 
			 of Frequency Steps must be within one frequency band 
			 range, but do not have to be in the same frequency band range 
			 as the MS TX Frequency Sequence. Ensure that none of the frequency 
			 values you've selected are NANs (9.91E+37)).
GPIB command: SETup:CFDTune:FREQuency:STEP:COUNt
You can specify up to 40 mobile station output power levels (indexed from 0 up to 39). You must use the MS TX Power Step Start Index and Number of Power Steps settings to specify which of these (consecutive) power levels are used for the MS TX Power Sequence.
Although you can enter any power levels between -129 and +80 dBm (because this measurement is common to the W-CDMA/HSDPA, 1xEV-DO and cdma2000 formats), when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only measure power levels in the range of -70 to +30 dBm and the measurement is only specified for power levels in the range of -61 to +28 dBm (these ranges assume an amplitude offset of 0; the ranges change as you change amplitude offsets, see Amplitude Offset ).
GPIB command: SETup:CFDTune:MS:TX:POWer:STEP[:LEVels]
You can specify up to 40 mobile station uplink frequencies (indexed from 0 up to 39). You must use the MS TX Frequency Step Start Index and Number of Frequency Steps settings to specify which of these (consecutive) frequencies (up to 20) are used for the MS TX Frequency Sequence.
Although you can enter any frequencies between 411 and 1980 MHz, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only test frequencies within a single W-CDMA/HSDPA frequency band range:
1000 to 1260 MHz
1260 to 1600 MHz
1600 to 2000 MHz
2000 to 2520 MHz
2520 to 3200 MHz
3200 to 4000 MHz
GPIB command: SETup:CFDTune:MS:TX:FREQuency:STEP[:VALues]
You can specify up to 40 test set output power levels (indexed from 0 up to 39). You must use the MS RX Power Step Start Index and Number of Power Steps settings to specify which of these (consecutive) power levels are used for the MS RX Power Sequence.
Although you can enter any power levels between -165 and 37 dBm, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, the test set can only transmit test power levels in the range of -109 to -15 dBm (RF IN/OUT ) or -109 to -7 dBm (RF OUT ONLY ). These ranges assume an amplitude offset of 0; the allowable ranges change as you change amplitude offsets, see Cell Power, AWGN Power and Total RF Power Ranges .
GPIB command: SETup:CFDTune:MS:RX:POWer:STEP[:LEVels]
You can specify up to 40 test set downlink frequencies (indexed from 0 up to 39). You must use the MS RX Frequency Step Start Index and Number of Frequency Steps settings to specify which of these (consecutive) frequencies (up to 20) are used for the MS RX Frequency Sequence.
Although you can enter any frequencies between 421 and 2170 MHz, when running the Fast Device Tune measurement in the W-CDMA/HSDPA application/format, you can only test frequencies within a single W-CDMA/HSDPA frequency band range:
1000 to 1260 MHz
1260 to 1600 MHz
1600 to 2000 MHz
2000 to 2520 MHz
2520 to 3200 MHz
3200 to 4000 MHz
GPIB command: SETup:CFDTune:MS:RX:FREQuency:STEP[:VALues]
The Fast Device Tune measurement results are currently only available via GPIB command (see FETCh:CFDTune ). Measurement results are not available on the front panel screen.
The test set performs a channel power measurement near the center of each step (7 ms after the start of the step), with a measurement interval of 666.7 us (1 timeslot) and the RRC Filter off. Power (dBm/5 MHz) is returned for each step in the MS TX Frequency/Power Series (except for the frequency re-tune steps). The total number of results returned by the measurement is always 400 (Number of Power Steps x Number of Frequency Steps power result values are returned, followed by 9.91E+37 (NAN) for all remaining values up to 400). The power results for the first frequency in the MS TX Frequency Sequence are returned first, then the power results for the second frequency in the MS TX Frequency Sequence, etc., followed by NANs if fewer than 400 points were measured.
Note that the test set does not report the mobile station's measurement results (for example, CPICH RSCP). You must capture the mobile station's measurement results so that you can compare its measurements with the test set's actual transmission levels.
The Fast Device Tune measurement meets specifications when the following input signal requirements are met:
 You must calibrate 
		 this measurement using the Calibrate 
		 Measurements procedure (see Calibrating 
		 the Test Set ).
Programming a Fast Device Tune Measurement
How Do I Make a Fast Device Tune Measurement?
Fast Device Tune Troubleshooting