This section is only applicable to a test application with the required feature license.
| Sets/queries the Number of blocks to test . | |
| Same as setting | |
| 1000 blocks | |
|
Test Application Revision: A.08 and above, with the required feature license
Test Application Revision: A.19.00 and above, with the required feature license.Extended the range from 99000 to 198000 |
|
OUTPUT 714;"SETup:HBLerror:COUNt 2000" ! Sets the Number of blocks to test to 2000 blocks. |
|
|
Sets/queries the Blocks to Test Specified Per Serving Cell .
When DC-HSDPA is configured and this setting is set to
When DC-HSDPA is configured and this setting is set to |
|
| Same as setting | |
| 0 (OFF) | |
|
Test Application Revision: A.19.00 and above, with the required feature license Lab Application Revision: H.01.00 and above. |
|
OUTPUT 714;"SETup:HBLerror:COUNt:DCHSdpa ON" |
|
Sets/queries
DC-HSDPA Serving Cell Blocks to Test
when DC-HSDPA is configured and the
Blocks to Test Specified Per Serving Cell
is set to
On
. |
|
| Same as setting | |
| 1000 blocks | |
|
Test Application Revision: A.19.00 and above, with the required feature license Lab Application Revision: H.01.00 and above. |
|
OUTPUT 714;"SETup:HBLerror:COUNt:DCHSdpa:SERVing 2000" ! Sets the Number of blocks to test for the serving cell to 2000 blocks. |
|
|
Sets/queries
DC-HSDPA Secondary Serving Cell Blocks to Test
when DC-HSDPA is configured and the
Blocks to Test Specified Per Serving Cell
is set to
If
Current Secondary Serving Cell Status
is |
|
| Same as setting | |
| 1000 blocks | |
|
Test Application Revision: A.19.00 and above, with the required feature license Lab Application Revision: H.01.00 and above. |
|
OUTPUT 714;"SETup:HBLerror:COUNt:DCHSdpa:SECondary 2000" ! Sets the Number of blocks to test for the secondary serving cell to 2000 blocks. |
|
|
The setting form of this command performs two functions: (1) sets the measurement's timeout value (see Measurement Timeouts ), and (2) sets the measurement's timeout state to 1 (on). |
|
| Same as setting | |
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"SETup:HBLerror:TIMeout 5" ! Sets measurement's timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the measurement's timeout state (see Measurement Timeouts ). |
|
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"SETup:HBLerror:TIMeout:STATe ON" ! Sets the measurement's timeout state to ON. |
|
|
Sets/queries the measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeouts ). |
|
|
Test Application Revision: A.08 and above, with the required feature license |
|
OUTPUT 714;"SETup:HBLerror:TIMeout:TIME 5" ! Sets the measurement's timeout to five seconds. |
|