DC-HSDPA Information

DC-HSDPA Information

Last updated: November 7, 2012

This section is only applicable to the lab application or a test application with the required feature license.

DC-HSDPA Information provides real-time statistics of several parameters. The statistics are accumulated over the number of blocks transferred since the current connection was established. When the maximum number of blocks is reached, the statistical data accumulation begins anew.

This information is most useful for troubleshooting or to determine the current status of your UE's behavior. For RF measurements over a specified number of blocks, see the HSDPA Block Error Ratio Measurement Description .

Manual Operation: When the required license is available, you can view the DC-HSDPA Information by pressing CALL SETUP -> Call Control 2 of 6 -> Additional Screens ( F1 ) -> HSDPA Information ( F4 ) -> DC-HSDPA Information ( F4 ).

These results are cleared by pressing Clear UE Info .

Secondary Serving Cell Status

DC-HSDPA Counters

The DC-HSDPA Information window displays counters to help you monitor the DC-HSDPA connection status. The results are continually updated in real time until the existing connection ends.

When one of the following events occurs, the counters reset to zero and then begin counting again.

DC-HSDPA information provides the following results:

DC-HSDPA Real Time Results with GPIB

Summary

Serving Cell Secondary Serving Cell
Block Error Ratio CALL:HSDPa:MS:REPorted:HBLerror:RATio? CALL:HSDPa:MS:REPorted:SCELl:HBLerror:RATio? CALL:HSDPa:MS:REPorted:SSCell:HBLerror:RATio?
Throughput CALL:HSDPa:MS:REPorted:IBTHroughput? CALL:HSDPa:MS:REPorted:SCELl:IBTHroughput? CALL:HSDPa:MS:REPorted:SSCell:IBTHroughput?
Blocks Transferred CALL:HSDPa:MS:REPorted:BLOCks? CALL:HSDPa:MS:REPorted:SCELl:BLOCks? CALL:HSDPa:MS:REPorted:SSCell:BLOCks?
ACKs Received CALL:HSDPa:MS:REPorted:ACK? CALL:HSDPa:MS:REPorted:SCELl:ACK? CALL:HSDPa:MS:REPorted:SSCell:ACK?
NACKs Received CALL:HSDPa:MS:REPorted:NACK? CALL:HSDPa:MS:REPorted:SCELl:NACK? CALL:HSDPa:MS:REPorted:SSCell:NACK?
statDTXs Received CALL:HSDPa:MS:REPorted:SDTX? CALL:HSDPa:MS:REPorted:SCELl:SDTX? CALL:HSDPa:MS:REPorted:SSCell:SDTX?
Count of Reported CQI Limitations CALL:STATus:REPorted:CQI:LIMitation:COUNt? CALL:STATus:REPorted:SCELl:CQI:LIMitation:COUNt? CALL:STATus:REPorted:SSCell:CQI:LIMitation:COUNt?
Last received CQI - CALL:HSDPa:MS:REPorted:SCELl:CQI[:LAST]?] CALL:HSDPa:MS:REPorted:SSCell:CQI[:LAST]?]
Maximum Allowed CQI

-

CALL:STATus:MAXimum:ALLowed:CQI:VALue? CALL:STATus:SSCell:MAXimum:ALLowed:CQI:VALue?
Test Mode User Def TB Size

-

CALL:STATus:HSDSchannel:TBSize? (Active Cell) or CALL:FDDTest:HSDSchannel:UDEFined:TBSize:INDex (FDD Test) CALL:STATus:SSCell:HSDSchannel:TBSize? (Active Cell) or CALL:FDDTest:SSCell:HSDSchannel:UDEFined:TBSize:INDex (FDD Test)
PS Data User Def TB Size

-

CALL:STATus:HSDSchannel:TBSize:PSData? CALL:STATus:SSCell:HSDSchannel:TBSize:PSData?
Last Signaled Measurement Power Offset

-

CALL:STATus:MPOWer:OFFSet:SIGNaled? CALL:STATus:SSCell:MPOWer:OFFSet:SIGNaled?

Related Topics


HSDPA Parameters

HSUPA Information and HSUPA Happy Bit Information