Last updated: January 16, 2009
|
Sets/queries the trigger arm state for the adjacent channel leakage measurement. The trigger arm state determines whether the adjacent channel leakage measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
OUTPUT 714;"SETUP:WACLEAKAGE:CONTINUOUS OFF" !Sets measurement to single trigger mode. |
|
|
The setting form of this command performs two functions: (1) sets the number of adjacent channel leakage measurements to be made in a multi-measurement, and (2) sets the multi-measurement STATe command to 1 (on). The query form returns the number of adjacent channel leakage multi-measurements to be made when multi-measurement state is ON. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| Off (10 when STATe = On) | |
OUTPUT 714;"SETUP:WACLEAKAGE:COUNT:SNUMBER 5" !Turns on multi-measurements and sets the number of measurements to 5. |
|
|
Sets/queries the number of adjacent channel leakage measurements to be made when the multi-measurement state is ON. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| 10 | |
OUTPUT 714;"SETUP:WACLEAKAGE:COUNT:NUMBER 5" !Sets the number of adjacent channel leakage multi-measurements to 5. |
|
|
Sets/queries the adjacent channel leakage multi-measurement state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
OUTPUT 714;"SETUP:WACLEAKAGE:COUNT:STATE ON" !Turns on adjacent channel leakage multi-measurements. |
|
|
Sets/queries the 1st lower adjacent channel's state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| 1 (on) | |
OUTPUT 714;"SETUP:WACLEAKAGE:LOW1:STATE 0" !Turns off the lower 1st adjacent channel. |
|
|
Sets/queries the 2nd lower adjacent channel's state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| 1 (on) | |
OUTPUT 714;"SETUP:WACLEAKAGE:LOW2:STATE 0" !Turns off the lower 2nd adjacent channel. |
|
|
The setting form of this command performs two functions: (1) sets the adjacent channel leakage measurement's timeout (see Measurement Timeouts ) value, and (2) sets the adjacent channel leakage measurement's timeout STATe to 1 (on). The query form returns the adjacent channel leakage measurement's timeout value. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
OUTPUT 714;"SETUP:WACLEAKAGE:TIMEOUT:STIME 5 S" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the adjacent channel leakage measurement's timeout (see Measurement Timeouts ) state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
OUTPUT 714;"SETUP:WACLEAKAGE:TIMEOUT:STATE ON" |
|
|
Sets/queries the adjacent channel leakage measurement's timeout (see Measurement Timeouts ) setting to be used when the timeout state is set to ON. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
OUTPUT 714;"SETUP:WACLEAKAGE:TIMEOUT:TIME 5 S" |
|
|
Sets/queries the ACLR measurement's HS-DPCCH Trigger Subframe Alignment setting.
This command is only applicable when
SETup:WACLeakage:TRIGger:SOURce
is set to |
|
| Same as setting | |
| 0 (subframe 0) | |
|
Test Application Revision: A.08 and above with the required feature license |
|
OUTPUT 714;"SETup:WACLeakage:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 1" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 1. |
|
|
Sets/queries the adjacent channel leakage measurement's Trigger Delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed. |
|
| Same as setting | |
|
Test or Lab Application Revision: A.01 and above Test Application Revision A.08 and Lab Application Revision A.03, increased range to -12 to 12 ms (previously it was -10 ms to 10 ms) |
|
OUTPUT 714;"SETUP:WACLEAKAGE:TRIGGER:DELAY 1MS" |
|
|
Sets/queries the adjacent channel leakage measurement's Trigger Source . |
|
| AUTO | |
|
Test or Lab Application Revision: A.01 and above Test Application Revision A.08 with the required feature license and Lab Application Revision A.03, added HSDPcchannel |
|
OUTPUT 714;"SETUP:WACLEAKAGE:TRIGGER:SOURCE IMMEDIATE" |
|
|
Sets/queries the 1st upper adjacent channel's state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| 1 (on) | |
OUTPUT 714;"SETUP:WACLEAKAGE:UPP1:STATE 0" !Turns off the upper 1st adjacent channel. |
|
|
Sets/queries the 2nd upper adjacent channel's state. See Adjacent Channel Leakage Ratio (ACLR) Measurement Description . |
|
| 1 (on) | |
OUTPUT 714;"SETUP:WACLEAKAGE:UPP2:STATE 0" !Turns off the upper 2nd adjacent channel. |
|