Last updated: January 16, 2009
|
Sets/queries the trigger arm state for the block error ratio measurement. The trigger arm state determines whether the block error ratio measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). See Trigger Arm (Single or Continuous) Description . |
|
|
Test Application Revision: A.05 and above Lab Application Revision: B.01 and above Test Application A.10 and Lab Application D.01, *RST setting changed to 0 (single). |
|
OUTPUT 714;"SETup:WBLerror:CONTinuous ON" ! Sets measurement to continuous trigger mode. |
|
| Sets/queries the number of blocks to test in the block error ratio test. See Number of Blocks to Test . | |
| 500 blocks | |
OUTPUT 714;"SETup:WBLerror:COUNt 1000" |
|
|
The setting form of this command performs two functions: (1) sets the block error ratio measurement's timeout (see Measurement Timeouts ) value, and (2) sets the block error ratio measurement's timeout STATe to 1 (on). The query form returns the block error ratio measurement's timeout value. |
|
| Same as setting | |
OUTPUT 714;"SETup:WBLerror:TIMeout 5" ! Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the block error ratio measurement's timeout state (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WBLerror:TIMeout:STATe ON" |
|
|
Sets/queries block error ratio measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WBLerror:TIMeout:TIME 5" |
|