Last updated: November 17, 2010
|
Sets/queries HS-DPCCH Measurement Interval . This command is only applicable when SETup:WCDomain:TRIGger:SOURce = HSDPcchannel.
The sum of |
|
| Same as setting | |
| 1.0 slot | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:INTerval:HSDPcchannel 0.8" ! Sets HS-DPCCH Measurement Interval to 0.8 slot. |
|
|
The setting form of this command performs two functions: (1) sets the code domain measurement's timeout (see Measurement Timeouts ) value, and (2) sets the adjacent channel leakage measurement's timeout STATe to 1 (on). The query form returns the loopback bit error rate measurement's timeout value. |
|
OUTPUT 714;"SETUP:WCDOMAIN:TIMEOUT:STIME 5 S" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the code domain measurement's timeout state (see Measurement Timeouts ). |
|
OUTPUT 714;"SETUP:WCDOMAIN:TIMEOUT:STATE ON" |
|
|
Sets/queries code domain measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeouts ). |
|
OUTPUT 714;"SETUP:WCDOMAIN:TIMEOUT:TIME 5 S" |
|
|
Sets/queries Transient Period . This command is only applicable when SETup:WCDomain:TRIGger:SOURce = HSDPcchannel. |
|
| INCL (include) | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:TRANsient EXCLude" ! Sets Transient Period to Exclude. |
|
|
Sets/queries HS-DPCCH Trigger Slot Alignment . This command is only applicable when SETup:WCDomain:TRIGger:SOURce = HSDPcchannel. |
|
| ACKN | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:TRIGger:ALIGnment:HSDPcchannel:SLOT CQI1" ! Sets HS-DPCCH Trigger Slot Alignment to CQI1. |
|
|
Sets/queries HS-DPCCH Trigger Subframe Alignment . This command is only applicable when SETup:WCDomain:TRIGger:SOURce = HSDPcchannel. |
|
| Same as setting | |
| 0 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 3" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 3. |
|
|
Sets/queries HS-DPCCH Trigger Subslot Alignment . This command is only applicable when SETup:WCDomain:TRIGger:SOURce = HSDPcchannel.
The sum of |
|
| Same as setting. | |
| 0.0 slot | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:TRIGger:ALIGnment:HSDPcchannel:SUBSlot 0.3" ! Sets HS-DPCCH Trigger Subslot Alignment to 0.3 slot. |
|
|
Sets/queries the code domain SFN Alignment setting. This setting is only applicable when SETup:WCDomain:TRIGger:SOURce is set to EFRame. |
|
| Same as setting. | |
| EVEN | |
|
Test Application Revision: A.12 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCDomain:TRIGger:ALIGnment:SFNumber EVEN" ! Sets SFN Alignment to Even |
|
|
Sets/queries Trigger Source . |
|
| AUTO | |
|
Test Application Revision: A.02 and above. Test Application Revision A.09, with the required feature license, added HSDPcchannel. Test Application Revision A.12 and above, with the required feature license, added EFRame. Lab Application Revision: A.01 and above. |
|
OUTPUT 714;"SETUP:WCDomain:TRIGGER:SOURCE AUTO" |
|
|
Sets/queries Timeslot . This command is only applicable when SETup:WCDomain:TRIGger:SOURce is NOT set to HSDPcchannel. |
|
| Same as setting | |
| 0 | |
OUTPUT 714;"SETUP:WCDOMAIN:TSLot 10" |
|