Show 

Home > Code Domain Measurement Description



Code Domain Measurement Description

Code Domain Measurement Description

Last updated: January 16, 2009

How is a Code Domain Measurement Made?

Code domain power (CDP) is an analysis of the distribution of signal power projected on a code-space of a particular dimension, normalized to the total signal power. To analyze the composite waveform, each channel is decoded using a code-correlation algorithm. This algorithm determines the correlation coefficient for each code. Once the channels are decoded, the power in each code channel is determined.

Code domain error (CDE) measurements are made by sampling the down-converted input signal, then applying DSP (Digital Signal Processing) techniques to determine the original data input to the UE transmitter's OVSF code spreading function for each channel. The DSP uses the original data and coding to generate a representation of the original waveform. This is the reference waveform for the code domain error measurements.

CDE is determined by comparing the reference waveform with the waveform being measured to determine the error vector. The error vector is projected onto the code domain at the same spreading factor used to determine CDP. The error vector for each power code is defined as the ratio to the mean power of the reference waveform expressed in dB.

Measurement Interval in Non-HSDPA Mode

When on a non-HSDPA connection, you must set Trigger Source to any value other than HS-DPCCH . When operating in this mode, the measurement is made during one timeslot (666.7 us). You can choose in which timeslot of the W-CDMA frame the measurement is performed using the Timeslot setting.

Timeslot Setting

Measurement Interval in HSDPA Mode

This section is only applicable to the lab application or feature-licensed test application .

To measure code domain on an HSDPA connection, you must set Trigger Source to HS-DPCCH . When Trigger Source is set to HS-DPCCH, you can specify the measurement interval and its placement within any of the 6 HSDPA subframes.

  1. Use the HS-DPCCH Trigger Subframe Alignment setting to choose in which 2 ms subframe (0 to 5) you want to place the measurement interval.
  2. Use the HS-DPCCH Trigger Slot Alignment setting to specify in which slot within the subframe you want to place the measurement interval ( AckNack = the first slot of the subframe, CQI1 = the second slot of the subframe and CQI2 = the third slot of the subframe).
  3. Set the duration of the measurement interval using the HS-DPCCH Measurement Interval setting. Note that the sum of HS-DPCCH Trigger Subslot Alignment and HS-DPCCH Measurement Interval cannot exceed 1.0 slot.
  4. Use the HS-DPCCH Trigger Subslot Alignment setting to specify where you want to place the measurement interval within the slot. You can place the measurement interval at the slot boundary, 0.1 slot (66.7 us) after the slot boundary, 0.2 slot (133.3 us) after the slot boundary... up to 0.5 slot (333.3 us) after the slot boundary. Note, however, that the sum of HS-DPCCH Trigger Subslot Alignment and HS-DPCCH Measurement Interval cannot exceed 1.0 slot. If you wish to place the measurement interval after the slot boundary using the HS-DPCCH Trigger Subslot Alignment setting, you must first decrease the HS-DPCCH Measurement Interval setting appropriately.
  5. You can choose to shorten the measurement interval so as to exclude the 25 us (96 chip) transient periods at the start and end of the measurement interval using the Transient Period setting. For example, if you set HS-DPCCH Measurement Interval to 0.5 slot (333.3 us or 1280 chips) and set Transient Period to Exclude , the measurement is performed over 283.3 us (or 1088 chips).

Measurement Interval Duration and Placement for HSDPA

Code Domain Measurement Parameters

HSDPA Measurement Parameters

This section is only applicable to the lab application or feature-licensed test application .

These settings are only applicable when Trigger Source = HS-DPCCH .

See Measurement Interval in HSDPA Mode for more information about using these parameters to specify the duration and placement of the measurement interval.

Code Domain Measurement Results

Code Domain Input Signal Requirements

Code Domain Measurement Calibration

This measurement should be calibrated using the Calibrate Measurements function ( CALibration:MEASurements? ) when the temperature has changed by ± 10° C or more since the last calibration. If this situation exists, the integrity indicator value becomes 19 and a message is displayed indicating "Uncalibrated Due to Temperature".

Related Topics