OUTPUT 714;"SETUP:WCPOWER:COUNT:STATE ON" !Turns on channel power multi-measurements. |
|
|
Sets/queries the state of the root-raised cosine (RRC) filter ( RRC Filter ). |
|
| OFF | |
OUTPUT 714;"SETUP:WCPOWER:FILTER:RRC ON" !Turns on the RRC filter. |
|
|
Sets/queries the channel power Measurement Interval . |
|
| Same as setting | |
|
Test or Lab Application Revision: A.01 and above Test Application Revision A.08 and Lab Application Revision A.03, increased range to 10 us to 12 ms (previously it was 0.1 ms to 10 ms) |
|
OUTPUT 714;"SETUP:WCPOWER:INTERVAL:TIME 10MS" !Sets interval time to 10 milliseconds. |
|
|
Sets/queries the channel power Manual Power Range Offset setting. This setting is only applicable when SETup:WCPower:RANGe:AUTO is set to off. |
|
| Same as setting. | |
|
Test Application Revision: A.12 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCPower:POWer:RANGe:OFFSet:MANual 0" ! Sets Manual Power Range Offset to 0 dB. |
|
|
Sets/queries the channel power Auto Range setting. |
|
| 1|0 | |
OUTPUT 714;"SETup:WCPower:RANGe:AUTO OFF" ! Sets Auto Range to Off. |
|
|
Sets/queries the channel power RMSCubed State . |
|
| 1|0 | |
|
Test Application Revision: A.12 and above, with the required feature license |
|
OUTPUT 714;"SETup:WCPower:RMSCubed:STATe OFF" ! Sets RMSCubed State to Off. |
|
|
The setting form of this command performs two functions: (1) sets the channel power measurement's timeout (see Measurement Timeouts ) value, and (2) sets the channel power measurement's timeout STATe to 1 (on). The query form returns the channel power measurement's timeout value. |
|
OUTPUT 714;"SETUP:WCPOWER:TIMEOUT:STIME 5 S" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the channel power measurement's timeout (see Measurement Timeouts ) state. |
|
OUTPUT 714;"SETUP:WCPOWER:TIMEOUT:STATE ON" |
|
|
Sets/queries the channel power measurement's timeout (see Measurement Timeouts ) setting to be used when the timeout state is set to ON. |
|
OUTPUT 714;"SETUP:WCPOWER:TIMEOUT:TIME 5 S" |
|
|
Sets/queries the channel power measurement's
HS-DPCCH Trigger Subframe Alignment
This command is only applicable when
SETup:WCPower:TRIGger:SOURce
is set to |
|
| Same as setting | |
| 0 (subframe 0) | |
|
Test Application Revision: A.08 and above with the required feature license |
|
OUTPUT 714;"SETup:WCPower:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 1" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 1. |
|
|
Sets/queries the channel power measurement's Trigger Delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed. |
|
| Same as setting | |
|
Test or Lab Application Revision: A.01 and above Test Application Revision A.08 and Lab Application Revision A.03, increased range to -12 to 12 ms (previously it was -10 ms to 10 ms) |
|
OUTPUT 714;"SETUP:WCPOWER:TRIGGER:DELAY 1MS" |
|
|
Sets/queries the channel power measurement's Trigger Source . |
|
| AUTO | |
|
Test or Lab Application Revision: A.01 and above Test Application Revision A.08 and Lab Application Revision A.03, added EXTernal Test Application Revision A.08 with the required feature license and Lab Application Revision A.03, added HSDPcchannel |
|
OUTPUT 714;"SETUP:WCPOWER:TRIGGER:SOURCE IMMEDIATE" |
|