Last updated: January 16, 2009
The channel power measurement is made on the RF input signal after frequency downconversion and an analog to digital conversion (see Block Diagram ). The actual power measurement is performed by the test set's digital signal processor (DSP).
When the RRC Filter for the channel power measurement is turned on, the results are typically about 0.25 dB lower than the thermal power measurement results.
Thermal power performance is only specified for signals down to -10 dBm, while the channel power measurement is able to accurately measure signals down to -61 dBm.
You must specify how you want to trigger the channel power measurement using the
Trigger Source
setting. You must also specify the
Measurement Interval
and may then choose to move the
Measurement Interval
relative to the trigger using the
Trigger Delay
setting.
For example (
for lab applications or feature-licensed test applications only
), given the following example power profile, to align the measurement trigger to measure the power level of the ACK portion of the HS-DPCCH signal (excluding the 25 us transient periods on either side of the slot boundaries), set
Trigger Source
to
HS-DPCCH
, set
HS-DPCCH Trigger Subframe Alignment
to
0
, set
Measurement Interval
to
616.7 us
and set
Trigger Delay
to
25 us
. To measure the power level of the statDTX, simply change
HS-DPCCH Trigger Subframe Alignment
to
3.
Multi-Measurement Count: (see Statistical Measurement Results ).
The signal can be filtered in the DSP with a root-raised cosine (RRC) filter with a rolloff of 0.22 and a bandwidth equal to the chip rate (3.84 MHz) to comply with 3GPP 34.121 conformance specifications that require RRC filtered power. The filter can also be turned off for conformance specifications requiring a mean power measurement. When the
RRC filter
is
Off
, the bandwidth of the channel power measurement is greater than (1+alpha) times the chiprate, where alpha=0.22.
Trigger Arm: (see Trigger Arm (Single or Continuous) Description ).
You may set
Trigger Source
to the following: (for more information on these trigger types, see
Trigger Source Description
).
Auto: if the UE is synchronized to the test set, it uses protocol triggering; otherwise, it uses immediate triggering.
External
This setting is only applicable to the lab application or a feature-licensed test application.
When
Trigger Source
is set to
HS-DPCCH
, you can specify on which uplink subframe the measurement triggers using the
HS-DPCCH Trigger Subframe Alignment
setting.
Trigger Source
can only be set to HS-DPCCH when
Channel Type
=
12.2k RMC + HSDPA
or
12.2k RMC + HSPA
.
Immediate
Protocol: Derived from the 10 ms downlink DPCH frame clock.
RF Rise
triggering can be used to measure power during PRACH bursts. The burst's on state level must be >-40 dBm and the off state level must be <-60 dBm for this trigger to work correctly.
You can move the
Measurement Interval
relative to the measurement trigger using the
Trigger Delay
setting. See
Triggering the Channel Power Measurement
.
This measurement can be made over a period of 10 us to 12 ms (the default is 1 timeslot or 666.7 us) by altering the
Measurement Interval
.
When
Auto Range
is set to on, the test set automatically determines the expected power level from the UE before performing a channel power measurement. However, note that the measurement takes longer to execute when
Auto Range
is set to on. Also, the UE's output power must be stable in order for the autoranging algorithm to operate properly.
When
Auto Range
is set to off, you must specify the expected power level from the UE as described in
Manual Power Range Offset
.
This setting is only applicable when
Auto Range
is off.
When
Auto Range
is off, the test set uses the
UE Target Power
setting (for automatic receiver power control) or the
Manual Power
setting (for manual receiver power control; see
Receiver Control
) to determine the expected power level from the UE. However, the
UE Target Power
setting (or
Manual Power
setting) only drives the DPCCH+DPDCH power level of the UE. When HS-DPCCH, E-DPCCH and/or E-DPDCH channels are present, the actual output power of the UE is greater than the
UE Target Power
setting. Thus when
Auto Range
is off, you must specify how much additional power is in the UE's signal due to the HSDPA and HSUPA channels (using the
Manual Power Range Offset
setting) to avoid an over range error.
Power Change Due to HS-DPCCH, E-DPCCH and E-DPDCH
= 10log
10
(Beta
c
^2 + Beta
d
^2 + Beta
hs
^2 + Beta
ec
^2 + Beta
ed
^2) - 10log
10
(Beta
d
^2 + Beta
c
^2). For example, for 34.121 v7.5.0 Table C.11.1.3 sub-test 1,
Power Change Due to HS-DPCCH, E-DPCCH and E-DPDCH
= 14 dB. Thus,
Manual Power Range Offset
should be set to 14 dB for sub-test 1 when
Auto Range
is off.
Manual Power Range Offset
should be set as follows for the other sub-tests - sub-test 2: 5 dB, sub-test 3: 13 dB, sub-test 4: 2 dB, sub-test 5: 16 dB.
Measurement Timeout: (see Measurement Timeouts ).
This setting is only applicable to the lab application or a feature-licensed test application.
When
Trigger Source
is set to
HS-DPCCH
, you can specify on which uplink subframe the measurement triggers. You can then use the
Trigger Delay
setting to move the
Measurement Interval
relative to that subframe boundary. See
Triggering the Channel Power Measurement
.
This setting is only available via GPIB command ( SETup:WCPower:RMSCubed:STATe ). This setting determines whether the RMSCubed measurement result is available.
This result is only available when RMSCubed State is set to on, and is only available via GPIB command. This result returns the root mean square of the cubic normalized voltage waveform (20log 10 ((v_norm 3 ) rms )), to aid in the calculation of CM (Cubic Metric) and MPR (Maximum Power Reduction) as defined in 3GPP TS 25.101 s6.2.2.
You must calibrate this measurement using the
Calibrate Measurements
procedure (see
Calibrating the Test Set
).