Last updated: January 16, 2009
|
Sets/queries the maximum power level expected from the UE's second power sequence in an Extended Range Dynamic Power measurement. See Second Sequence Expected Power for details. |
|
| Same as setting | |
| -14 dBm | |
OUTPUT 714;"SETup:WEDPower:SSEQuence:EXPected:POWer -5" ! Sets the second sequence expected power to -5 dBm. |
|
|
Sets/queries the number of steps to be measured in the first power sequence in an Extended Range Dynamic Power measurement. The sum of the first power sequence steps (specified by this command) and the second power sequence steps (specified by SETup:WEDPower:STEPs:SSEQuence ) can not be more than 85 steps. See First Sequence Steps for details. |
|
| Same as setting | |
| 38 | |
OUTPUT 714;"SETup:WEDPower:STEPs:FSEQuence 5" ! Sets the number of power steps in the first sequence to 5. |
|
|
Sets/queries the number of steps to be measured in the second power sequence in an Extended Range Dynamic Power measurement. The sum of the first power sequence steps (specified by SETup:WEDPower:STEPs:FSEQuence ) and the second power sequence steps (specified by this command) can not be more than 85 steps. See Second Sequence Steps . |
|
| Same as setting | |
| 38 | |
OUTPUT 714;"SETup:WEDPower:STEPs:SSEQuence 5" ! Sets the number of power steps in the second sequence to 5. |
|
|
The setting form of this command performs two functions: (1) sets the measurement timeout value (see SETup:WEDPower:TIMeout:TIME ), and (2) sets the measurement timeout state to on (see SETup:WEDPower:TIMeout:STATe ). Ensure that you set the measurement timeout to a value great enough to allow you to command the UE to transmit its power sequences and for the test set to measure the power sequences. The query form of this command returns the measurement timeout value. See Measurement Timeouts . |
|
| Same as setting | |
OUTPUT 714;"SETup:WEDPower:TIMeout 5" ! Sets timeout state to on and the timeout time to 5 seconds. |
|
|
Sets/queries the measurement timeout state for the Extended Range Dynamic Power measurement. The measurement timeout state can also be set to on using the SETup:WEDPower:TIMeout[:STIMe] command. See Measurement Timeouts . |
|
OUTPUT 714;"SETup:WEDPower:TIMeout:STATe ON" |
|
|
Sets/queries the measurement timeout value for the Extended Range Dynamic Power measurement. It is used when the timeout state is set to on. The measurement timeout value can also be set using the SETup:WEDPower:TIMeout[:STIMe] command. Ensure that you set the measurement timeout to a value great enough to allow you to command the UE to transmit its power sequences and for the test set to measure the power sequences. See Measurement Timeouts . |
|
| Same as setting | |
OUTPUT 714;"SETup:WEDPower:TIMeout:TIME 5" |
|
|
Sets/queries the trigger delay for an Extended Range Dynamic Power measurement. It is applicable when SETup:WEDPower:TRIGger:SOURce is set to EXTernal. See Trigger Delay for details. |
|
| Same as setting | |
| 1.66667E-4 s (166.667 us) | |
OUTPUT 714;"SETup:WEDPower:TRIGger:DELay 200 US" ! Sets trigger delay to 200 microseconds. |
|
|
Sets/queries the trigger source for an Extended Range Dynamic Power measurement. See Trigger Source for details. |
|
| RISE | |
OUTPUT 714;"SETup:WDPAnalysis:TRIGger:SOURce EXTernal" ! Sets the trigger source to external |
|
|
Sets/queries the RF rise trigger threshold for an Extended Range Dynamic Power measurement. It is applicable when SETup:WEDPower:TRIGger:SOURce is set to RISE. See RF Rise Trigger Threshold for details. |
|
| Same as setting | |
| 0 dBm | |
OUTPUT 714;"SETup:WEDPower:TRIGger:THReshold 10" ! Sets the RF rise trigger threshold to 10 dBm. |
|