Last updated: January 16, 2009
The Extended Range Dynamic Power measurement allows you to measure the UE's transmitter output power across its entire dynamic power (up to 90 dB) in one measurement cycle. This measurement does not require a call established between the test set and UE since it does not utilize any overhead signalling to control the UE's power or frequency. Rather, you must place your UE into a test mode which forces it to transmit two power sequences you desire to test, and then analyze the resulting UE output power using the test set.
The Extended Range Dynamic Power measurement can measure power between -61 dBm and +28 dBm. Two power sequences output from the UE can be measured in one measurement cycle and the power range of each power sequence must not span more than 45 dB. Therefore, to measure a power range greater than 45 dB, you must break the power range up into two power sequences that do not exceed 45 dB. Each power sequence can contain up to 84 power steps (the levels can step up and/or down with varying magnitudes of change and the length of each step is fixed to one timeslot (666.7 us)). The sum of the steps in the two power sequences can not exceed 85 power steps. Moreover, you must command your UE to transmit for 15 power steps (timeslots) with constant or varied power levels between the two power sequences you desire to measure because the measurement must re-range its receiver in the middle of the two power sequences. The test set does not make any power measurements during the 15 timeslots re-range period. For example, to measure a UE's output power ranging from +24 dBm to -51 dBm, it is recommended that you command your UE to output the first power sequence stepping through the range of +24 dBm to -13 dBm in 1 dB step size, then hold its power constant for 15 timeslots, and then output the second power sequence stepping through the power range of -14 dBm to -51 dBm in 1 dB step size. The test set measures a total of 76 steps (timeslots) in one measurement and returns 76 power results for each step.
The figure below shows a typical example of UE output power sequence for the Extended Range Dynamic Power measurement.
The Extended Range Dynamic Power measurement can be made in Active Cell Operating Mode or FDD Test Operating Mode . Before starting the measurement, you must first set Measurement Frequency to the expected UE transmitter frequency and set Manual Power to the maximum expected power. To best utilize the 45 dB dynamic range of the test set's receiver, Manual Power should be set to the highest power expected in the first power sequence and Second Sequence Expected Power should be set to the highest power expected in the second power sequence. You must specify the number of steps in both sequences ( First Sequence Steps and Second Sequence Steps ), configure the trigger ( Trigger Source , RF Rise Trigger Threshold or Trigger Delay ), initiate the measurement, then order the UE to send its power sequences.
When the Extended Range Dynamic Power measurement is initiated, it waits for an RF rise trigger from the UE or an external trigger (see
Triggering the Extended Range Dynamic Power Measurement
). Once triggered, the test set starts to measure the UE output power sequences. It first samples the signals for the number of steps (timeslots) specified by the
First Sequence Steps
, then re-ranges its receiver according to the setting of
Second Sequence Expected Power
during the next 15 timeslots re-range period (the test set does not make any measurement during the re-range period), and after that, samples the signal for the number of timeslots specified by the
Second Sequence Steps
. When all of the power steps in both power sequences are sampled (with RRC filter off), the test set analyzes the power of each step and then returns the power results for all measured steps. The power result of each step is determined by averaging over a half timeslot measurement interval (0.5 timeslot = 333.3 us). When the
Trigger Source
is
RF Rise
, the measurement interval is centered in the middle of each step (666.7 us). That is, the measurement interval shall be at 166.7 us relative to the start of each step. When the
Trigger Source
is
External
, you can use the
Trigger Delay
to specify when the measurement interval should begin.
The measurement can be triggered externally or by an RF rise trigger in the power sequence.
RF Rise
and specifying the appropriate
RF Rise Trigger Threshold
. To ensure a successful RF rise triggering, it is recommended that you do the following:
Manual
and set
Manual Power
to the highest power expected in the first power sequence. It is also recommended that the
RF Rise Trigger Threshold
be set to approximately 10 dB below the highest power expected in the first power sequence.
RF Rise Trigger Threshold
level. If the first power step you desire to measure meets the trigger pulse requirements, no separate trigger pulse is needed. Otherwise, you should include a separate power step as a trigger pulse in the first power sequence that you desire to measure.
RF Rise Trigger Threshold
level, this causes the measurement to be triggered on an RF rise signal.
External
as needed for your test cases. When
External
is selected as your trigger source, you are allowed to adjust the
Trigger Delay
.Sets the number of steps (1 to 84) the UE will transmit during the first power sequence. The length of each step is fixed to one timeslot (666.7us). The UE's output power steps up or down through the first power sequence, which must not exceed 45 dB power range.
Note: The sum of First Sequence Steps and Second Sequence Steps can not be more than 85 steps.
GPIB command: SETup:WEDPower:STEPs:FSEQuence
Sets the number of steps (1 to 84) the UE will transmit during the second power sequence. The length of each step is fixed to one timeslot (666.7us). The UE's output power steps up or down through the second power sequence, which must not exceed 45 dB power range.
Note: The sum of the First Sequence Steps and Second Sequence Steps can not be more than 85 steps.
GPIB command: SETup:WEDPower:STEPs:SSEQuence
Sets the maximum expected power that the UE will transmit during the second power sequence. It should be set to the highest power in the second power sequence to best utilize the 45 dB dynamic range of the receiver.
The test set ranges its receiver based on the
Manual Power
setting for the first power sequence measurement (it is recommended you set the
Manual Power
to the highese power in the first power sequence) and then re-ranges it receiver based on the
Second Sequence Expected Power
setting for the second power sequence.
GPIB command: SETup:WEDPower:SSEQuence:EXPected:POWer
This setting is only applicable when the
Trigger Source
is set to
RF Rise
. When the
Trigger Source
is set to
RF Rise
, you must set the
RF Rise Trigger Threshold
to the power level (in dBm) at which you want the measurement to trigger. When the power of the UE's signal rises above the
RF Rise Trigger Threshold
level, the measurement is triggered.
The
RF Rise Trigger Threshold
must be set to within 0 dB to -25 dB of
Manual Power
(it is suggested that you set
Manual Power
to the highest power level of the first power sequence to best utilize the 45 dB dynamic range of the receiver). Also, it is recommended that the
RF Rise Trigger Threshold
be set to approximately 10 dB below the
Manual Power
.
The test set assumes a crest factor of 3.1 dB for the signal (as is typical for an uplink DPCH signal relative to a CW signal) and thus actually triggers when the input signal reaches the
RF Rise Trigger Threshold
level plus 3.1 dB. If the UE's signal has a crest factor other than 3.1 dB, you must set the
RF Rise Trigger Threshold
level accordingly.
GPIB command: SETup:WEDPower:TRIGger:THReshold
You may set
Trigger Source
to
RF Rise
or External
. If
Trigger Source
is set to
RF Rise
, you must characterize the trigger using the
RF Rise Trigger Threshold
.
For more information on these trigger types, see Trigger Source Description .
GPIB command: SETup:WEDPower:TRIGger:SOURce
The power level of each step is measured by averaging over a half timeslot measurement interval (0.5 timeslot = 333.3 us). When the
Trigger Source
is
External
, you can move the measurement interval of the first power step relative to the external trigger using the
Trigger Delay
setting. The measurement intervals for all subsequent steps are then spaced by one timeslot. To make the power measurement of each step always be centered in the middle of the step, you should set the
Trigger Delay
to the time offset between the external trigger and the start of the first power step plus 166.7 us.
When the
Trigger Source
is
RF Rise
, the power measurement is averaged over 0.5 timeslot measurement interval (333.3 us) that is always centered in the middle of each step. Therefore, the measurement interval starts at 166.7us relative to the start of each step.
For example, if the UE began to output its power sequences at 200 us delay after the external trigger, you should set
Trigger Source
to
External
and
Trigger Delay
to
366.7 us
. Thus, the power of each step is averaged for a half timeslot (333.3 us) that is centered in the middle of the step (since the length of each step is fixed to one timeslot (666.7 us) and the measurement interval is fixed to half timeslot (333.3 us)).
GPIB command: SETup:WEDPower:TRIGger:DELay
Measurement Timeout
to a value great enough to allow you to command the UE to transmit its power sequences and for the test set to measure the power sequences.GPIB command: SETup:WEDPower:TIMeout[:STIMe]
The number of steps measured should be the sum of the First Sequence Steps and Second Sequence Steps settings. It can be queried using the FETCh:WEDPower or FETCh:WEDPower:STEPs command (see FETCh:WEDPower ). It is also displayed on the front panel graphical display (see the figure below).
The test set measures the average power for each step by performing a channel power measurement (with RRC filter off) over a measurement interval of 333.3 us (one half timeslot). The measurement interval is centered in the middle of the 666.7 us (timeslot) step when
Trigger Source
is
RF Rise
, or is offset from the start of the step according to the
Trigger Delay
setting when
Trigger Source
is set to
External
.
You can retrieve the average power measured for each step using the FETCh:WEDPower command or from the front panel (see the figure below).
The Extended Range Dynamic Power measurement can measure power between -61 dBm and +28 dBm.
The dynamic range for each power sequence is 45 dB. That is, the UE's power can not vary by more than 45 dB in any of the two power sequences.
You must calibrate this measurement using the measurement calibration procedure (see Calibrating the Test Set ).
Manual Operation: How Do I Make an Extended Range Dynamic Power Measurement?
Programming an Extended Range Dynamic Power Measurement
Extended Range Dynamic Power Measurement Troubleshooting