SETup:WOOSynch
This section is only applicable to the lab application.
Last updated: January 16, 2009
GPIB Command Conventions
SETup:WOOSynch:INTerval:AB
|
Function
|
Sets/queries
Segment Ta-b Interval
. |
|
Setting
|
Range: 0.04 to 5.00 seconds
Resolution: 0.04 seconds
|
|
Query
|
Same as setting |
|
*RST Setting
|
5.00 seconds |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:INTerval:AB 3.5"
! Sets Segment Ta-b Interval to 3.52 s (because the resolution is 0.04 seconds).
|
SETup:WOOSynch:INTerval:CD
|
Function
|
Sets/queries
Segment Tc-d Interval
. |
|
Setting
|
Range: 0.04 to 5.00 seconds
Resolution: 0.04 seconds
|
|
Query
|
Same as setting |
|
*RST Setting
|
5.00 seconds |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:INTerval:CD 3.5"
! Sets Segment Tc-d Interval to 3.52 s (because the resolution is 0.04 seconds).
|
SETup:WOOSynch:INTerval:DE
|
Function
|
Sets/queries
Segment Td-e Interval
. |
|
Setting
|
Range: 0.04 to 5.00 seconds
Resolution: 0.04 seconds
|
|
Query
|
Same as setting |
|
*RST Setting
|
5.00 seconds |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:INTerval:DE 3.5"
! Sets Segment Td-e Interval to 3.52 s (because the resolution is 0.04 seconds).
|
SETup:WOOSynch:RATio:AB
|
Function
|
Sets/queries
DPCCH Quality Ratio Qa-b
. |
|
Setting
|
Range: -10.0 to -30.0 dB
Resolution: 0.1 dB
|
|
Query
|
Same as setting |
|
*RST Setting
|
-21.6 dB |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:RAT:AB -22.0"
! Sets DPCCH Quality Ratio Qa-b to -22.0 dB.
|
SETup:WOOSynch:RATio:BD
|
Function
|
Sets/queries
DPCCH Quality Ratio Qb-d
. |
|
Setting
|
Range: -10.0 to -30.0 dB
Resolution: 0.1 dB
|
|
Query
|
Same as setting |
|
*RST Setting
|
-28.40 dB |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:RATio:BD -28.0"
! Sets DPCCH Quality Ratio Qb-d to -28.0 dB.
|
SETup:WOOSynch:RATio:DE
|
Function
|
Sets/queries
DPCCH Quality Ratio Qd-e
. |
|
Setting
|
Range: -10.0 to -30.0 dB
Resolution: 0.1 dB
|
|
Query
|
Same as setting |
|
*RST Setting
|
-24.40 dB |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:RATio:DE -24.0"
! Sets DPCCH Quality Ratio Qd-e to -24.0 dB.
|
SETup:WOOSynch:RATio:E
|
Function
|
Sets/queries
DPCCH Quality Ratio Qe+
. |
|
Setting
|
Range: -10.0 to -30.0 dB
Resolution: 0.1 dB
|
|
Query
|
Same as setting |
|
*RST Setting
|
-17.60 dB |
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:RATio:E -18.0"
! Sets DPCCH Quality Ratio Qe+ to -18.0 dB.
|
SETup:WOOSynch:TIMeout[:STIMe]
|
Function
|
The setting form of this command performs two functions: (1) sets the measurement's timeout (see
Measurement Timeouts
) value, and (2) sets the measurement's timeout STATe to 1 (on).
The query form returns the measurement's timeout value.
|
|
Setting
|
Range: 0.1 to 999.9 seconds
Resolution: 0.1 second
|
|
Query
|
Same as setting |
|
*RST Setting
|
20 seconds, (off)
|
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:TIMeout 5"
! Sets timeout state to ON and sets the timeout time to 5 seconds.
|
SETup:WOOSynch:TIMeout:STATe
|
Function
|
Sets/queries the measurement's timeout state (see
Measurement Timeouts
).
|
|
Setting
|
Range: 1|ON|0|OFF
|
|
Query
|
Range: 1|0
|
|
*RST Setting
|
0 (off)
|
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:TIMeout:STATe ON"
! Sets the measurement's timeout state to ON.
|
SETup:WOOSynch:TIMeout:TIME
|
Function
|
Sets/queries the measurement's timeout setting to be used when the timeout state is set to ON (see
Measurement Timeouts
).
|
|
Setting
|
Range: 0.1 to 999.9 seconds
Resolution: 0.1 second
|
|
Query
|
Same as setting
|
|
*RST Setting
|
20 seconds
|
|
Requirements
|
Lab Application Revision: C.01 and above
|
|
Programming Example
OUTPUT 714;"SETup:WOOSynch:TIMeout:TIME 5"
! Sets the measurement's timeout to five seconds.
|