Last updated: November 12, 2010
|
Sets/queries the Measurement Interval .
This setting is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
|
Test Application Revision: A.05 and above Test Application Revision A.06 changed range upper limit from 75 to 90 Lab Application Revision: B.01 and above Lab Application Revision C.01 changed range upper limit from 75 to 90 |
|
OUTPUT 714;"SETup:WPDiscon:INTerval 6" ! Sets the measurement interval to 6 slots. |
|
|
Sets/queries the Number of Pattern Repetitions .
This setting is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
OUTPUT 714;"SETup:WPDiscon:NPRepetition 10" ! Sets the Number of Pattern Repetitions to 10. |
|
|
Sets/queries the Power Control Pattern .
This setting is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
|
Test Application Revision: A.06 and above Test Application Revision A.09 added DN18 and UP18 |
|
OUTPUT 714;"SETup:WPDiscon:PCPattern DN5_4UP" ! Sets the Power Control Pattern to 5DOWN/4UP. |
|
|
Sets/queries the Reference Timeslot .
This setting is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
| 0 | |
OUTPUT 714;"SETup:WPDiscon:RTIMeslot 8" ! Sets the reference timeslot to the 9th slot of the first available frame. |
|
|
Sets/queries HS-DPCCH Measurement Step Count .
This command is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
| 21 | |
|
Test Application Revision: A.10 and above with the required feature license |
|
OUTPUT 714;"SETup:WPDiscon:STEP:COUNt 90" ! Sets HS-DPCCH Measurement Step Count to 90. |
|
|
Sets/queries HS-DPCCH Measurement Step Interval .
This command is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to
The sum of |
|
| Same as setting. | |
| 0.5 slot | |
|
Test Application Revision: A.10 and above with the required feature license |
|
OUTPUT 714;"SETup:WPDiscon:STEP:INTerval 1.0" ! Sets HS-DPCCH Measurement Step Interval to 1.0 slot. |
|
|
The setting form of this command performs two functions: (1) sets the phase discontinuity measurement's timeout (see Measurement Timeouts ) value, and (2) sets the phase discontinuity measurement's timeout STATe to 1 (on). The query form returns the phase discontinuity measurement's timeout value. |
|
| Same as setting | |
OUTPUT 714;"SETup:WPDiscon:TIMeout 5" ! Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the phase discontinuity measurement's timeout state (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WPDiscon:TIMeout:STATe ON" ! Sets the phase discontinuity measurement's timeout state to ON. |
|
|
Sets/queries the phase discontinuity measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WPDiscon:TIMeout:TIME 5" ! Sets the phase discontinuity measurement's timeout to five seconds. |
|
|
Sets/queries HS-DPCCH Trigger Slot Alignment .
This command is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Range: ACKN|CQI1|CQI2 | |
| ACKN | |
|
Test Application Revision: A.10 and above with the required feature license |
|
OUTPUT 714;"SETup:WPDiscon:TRIGger:ALIGnment:HSDPcchannel:SLOT CQI2" ! Sets HS-DPCCH Trigger Slot Alignment to CQI2. |
|
|
Sets/queries HS-DPCCH Trigger Subframe Alignment .
This command is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to |
|
| Same as setting. | |
| 0 | |
|
Test Application Revision: A.10 and above with the required feature license |
|
OUTPUT 714;"SETup:WPDiscon:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 5" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 5. |
|
|
Sets/queries HS-DPCCH Trigger Subslot Alignment .
This command is only applicable when
SETup:WPDiscon:TRIGger:SOURce
is set to
The sum of |
|
| Same as setting. | |
| 0.0 slot | |
|
Test Application Revision: A.10 and above with the required feature license |
|
OUTPUT 714;"SETup:WPDiscon:TRIGger:ALIGnment:HSDPcchannel:SUBSlot 0.5" ! Sets HS-DPCCH Trigger Subslot Alignment to 0.5 slot. |
|
|
Sets/queries the Trigger Source . |
|
| PROT | |
|
Test Application Revision: A.05 and above Test Application Revision A.06 changed *RST setting from AUTO to PROT Test Application Revision A.10 with required feature license, added HSDPcchannel Lab Application Revision: B.01 and above Lab Application Revision C.01 changed *RST setting from AUTO to PROT |
|
OUTPUT 714;"SETup:WPDiscon:TRIGger:SOURce PROTocol" ! Sets the phase discontinuity measurement trigger source to PROTocol. |
|