Last updated: October 26, 2010
|
Sets/queries the trigger arm state for the PESQ measurement. See PESQ Measurement Parameters . |
|
|
Lab Application Revision: G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:CONTinuous OFF" !Sets measurement to single trigger mode. |
|
|
Sets/queries the Expected Audio In Peak Voltage that is applied at the test set's AUDIO IN connector for the PESQ measurement. The units (V|mV|uV) are optional. If no units are specified, then units default to V. See PESQ Measurement Parameters . |
|
| 2.0 V | |
|
Lab Application Revision G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:INPut:VOLTage 2" !Sets the PESQ Expected Audio In Peak Voltage to 2 V. |
|
|
Sets/queries the measurement mode used by the PESQ measurements. See PESQ Measurement Parameters . |
|
| BOTH | |
|
Lab Application Revision: G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:MEASurement:MODE UPL" !Sets the PESQ measurement mode to Uplink audio. |
|
|
Sets/queries the PESQ Maximum Audio Out Peak voltage. The units (V|mV|uV) are optional. If no units are specified, then units default to V. See PESQ Measurement Parameters . |
|
| 0.0 V | |
|
Lab Application Revision: G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:OUTPut:VOLTage 0.0" ! Sets the PESQ Maximum Audio Out Peak voltage. |
|
|
Sets/queries the speech source of the PESQ measurement. See PESQ Measurement Parameters . |
|
| MALE | |
|
Lab Application Revision: G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:SPEech MALE" !Sets the PESQ speech source to Male. |
|
|
Lab Application Revision: G.00 and above |
|
OUTPUT 714;"SETup:WPESquality:TIMeout:STATe ON" |
|