Last updated: October 26, 2010
This section is only applicable to the feature-licensed lab application or test application
Perceptual Evaluation of Speech Quality (PESQ), as defined in the ITU-T P.862 standard, is a objective method to test the speech quality of the mobile station. The objectivity is based on the comparison to the traditional MOS (Mean Opinion Score) method in which a group of listeners are used to rate the voice quality to a value ranging from 1(bad) to 5 (excellent).
When
AMR Voice
is selected as the paging service (see
Paging Service
), the
AMR Source
is set to PESQ and the
AMR Radio Access Bearer
is set to a desired vocoder (see
AMR Setup
), the test set supports the PESQ measurement by comparing the original signal with the received signal passed through a communication system. After the PESQ analysis, a score is given ranging from -0.5 to 4.5. A higher score means a better speech quality.
There are three modes provided for this measurement: Uplink Audio, Downlink Audio and Both.
The parameters shown in the PESQ Setup menu include:
Uplink Audio
is selected, the test set generates the original signal and analyzes the received uplink signal from the mobile to perform the PESQ measurement. When
Downlink Audio
is selected, the test set generates the original signal and analyzes the signal at its
AUDIO IN
port. If the
Measurement Mode
is set to Both, the test set performs the uplink and the downlink PESQ measurement simultaneously. GPIB Command: SETup:WPESquality:MEASurement:MODE
Male
and
Female
.GPIB Command: SETup:WPESquality:SPEech
GPIB Command: SETup:WPESquality:INPut:VOLTage[:EXPected]
GPIB Command: SETup:WPESquality:OUTPut:VOLTage[:MAXimum]
GPIB Command: SETup:WPESquality:CONTinuous
GPIB Command: SETup:WPESquality:TIMeout[:STIMe]
In Progress
or
Completed
. GPIB Commands: SETup:WPESquality , FETCh:WPESquality .
Measuring Perceptual Evaluation of Speech Quality (PESQ)
Perceptual Evaluation of Speech Quality Measurement Troubleshooting