Last updated: January 16, 2009
This section is only applicable to the lab application.
|
Sets/queries the Transient Period setting. |
|
OUTPUT 714;"SETup:WPPAnalysis:TRANsient EXCLude" ! Excludes PRACH preamble transient periods from PRACH analysis. |
|
| Sets/queries the Trigger Delay . This setting is applied only when SETup:WPPAnalysis:TRIGger:SOURce is set to RISE. | |
| 0 chips | |
OUTPUT 714;"SETup:WPPAnalysis:Trigger:DELay 284" |
|
| Sets/queries the Trigger Source . | |
| PROT | |
OUTPUT 714;"SETup:WPPAnalysis:TRIGger:SOURce RISE" ! Sets the PRACH preamble analysis trigger to RF rise. |
|
|
The setting form of this command performs two functions: (1) sets the PRACH preamble analysis timeout (see Measurement Timeouts ) value, and (2) sets the PRACH preamble analysis timeout STATe to 1 (on). The query form returns the PRACH preamble analysis timeout value. |
|
| Same as setting | |
OUTPUT 714;"SETup:WPPAnalysis:TIMeout 5" ! Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the PRACH preamble analysis timeout state (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WPPAnalysis:TIMeout:STATe ON" ! Sets the timeout state to ON. |
|
|
Sets/queries PRACH preamble analysis timeout setting to be used when the timeout state is set to ON (see Measurement Timeouts ). |
|
OUTPUT 714;"SETup:WPPAnalysis:TIMeout:TIME 5" ! Sets the timeout to 5 seconds. |
|