Last updated: January 16, 2009
This section is only applicable to the lab application.
3GPP TS 25.101, 6.8 states "Transmit modulation defines the modulation quality for expected in-channel RF transmissions from the UE. The requirements apply to all transmissions including the PRACH/PCPCH pre-amble and message parts and all other expected transmissions. In cases where the mean power of the RF signal is allowed to change versus time e.g. PRACH, DPCH in compressed mode, change of TFC and inner loop power control, the EVM and Peak Code Domain Error requirements do not apply during the 25 us period before and after the nominal time when the power is expected to change."
The PRACH preamble analysis measurement determines the modulation and timing errors between the transmitted signal of the UE and the ideal signal. The measurement algorithm is similar to that used in the waveform quality and IQ tuning measurements (see Waveform Quality Measurement Description and IQ Tuning Measurement Description ), except that the measurement is performed on a PRACH preamble burst, rather than over a timeslot of the DPCH transmission.
You can choose whether to include the "transient periods" of 96 chips (25 us) on either side of the PRACH preamble in the measurement using the Transient Period setting (for all measurement results except Relative Power (in dB) ). The measurement can thus be performed over the entire PRACH preamble burst, (4096 chips, or 1066.7 us), or only over 3904 chips (1016.7 us).
 
Before initiating a PRACH preamble analysis measurement, turn the UE on and wait for it to camp to the test set's signal. When you initiate the PRACH preamble measurement by pressing
 START SINGLE 
or sending the 
INITiate
 command, the test set sets 
Call Limit State
 to
 On 
to prevent successful call connection, then pages the UE (the test set returns
 Call Limit State 
to its prior setting after completion of the measurement). This forces the UE to transmit PRACH preamble bursts.
After the measurement is triggered by a burst (see Trigger Source ) it must determine which signature the UE used to transmit the PRACH preamble so that it can decode the burst data. To do this, it attempts to correlate the data to each of the signatures specified by the PRACH Signature setting. The measurement will execute fastest if you only specify one available signature.
When operating in FDD Test Operating Mode , you do not have access to the PRACH Signature setting, as the test set does not send this type of signalling to the UE in FDD test operating mode. However, when you initiate the measurement in FDD test operating mode, the measurement uses the value last set in the PRACH signature setting to determine which signatures to try to correlate to the PRACH preamble burst. Thus, before running this measurement in FDD test operating mode, you must switch to Active Cell Operating Mode and ensure that the PRACH Signature setting includes the signature that your UE will transmit.
To perform the PRACH preamble analysis measurement, you must set Available Subchannels (Bit Mask) to only allow one available subchannel.
 
You must also set 
PRACH Preambles
 to at least 3 before initiating this measurement. It is recommended that you set
 PRACH Preambles 
to
 3
, 
PRACH Ramping Cycles (MMAX)
 to
 1
, and 
Call Limit State
 to
 Off 
before initiating this measurement to minimize issues after the measurement has completed. See the following: 
No other measurements can be running when a PRACH preamble analysis measurement is performed. If any measurements are running when a PRACH preamble analysis measurement is initiated, they are closed and a message is displayed to indicate that they were closed.
 
You can set
 Trigger Source 
as follows:
Protocol
: If trigger source is set to protocol, the test set monitors every available access slot (as determined by the 
Available Subchannels (Bit Mask)
 setting) to see if a significant change in power occurs (which would indicate a PRACH preamble burst is present in that access slot). If a burst is present, the measurement is triggered on the access slot boundary.
External
: see 
Trigger Source Description
.
RF Rise
: If trigger source is set to RF rise, the measurement is triggered when the UE's power rises to within 9 dB of the expected power (the expected power is equal to 
Initial PRACH TX Power
 if
 Power Control 
is set to
 Auto
, or
 Manual Power 
if
 Power Control 
is set to
 Manual
; see 
Receiver Control
). When Trigger Source is set to RF Rise, you may specify a 
Trigger Delay
. When trigger source is set to RF rise, the 
Timing Error (in chips)
 result is not available.Trigger delay is only available when Trigger Source is set to RF Rise. The trigger delay setting specifies when to begin the measurement relative to the trigger event. If trigger delay is set to 0 chips, the measurement will begin immediately after the trigger event. See Trigger Delay Description for additional information about trigger delays.
 
The transient period setting determines whether to include the "transient periods" of 96 chips (25 us) on either side of the PRACH preamble in the measurement. If
 Transient Period 
is set to
 Include
, the measurement is performed over the entire PRACH preamble, 4096 chips (1066.7 us). If
 Transient Period 
is set to
 Exclude
, the measurement is performed over only 3904 chips (1016.7 us).
Relative Power 
is always measured over 4096 chips.This result is the rms EVM for the entire PRACH preamble burst (either 4096 or 3904 chips, depending upon the Transient Period setting).
The EVM for each chip measured in the burst is also available (see EVM (in %) ).
This result is the worst EVM reported for any chip in the burst (either 3904 or 4096 chips are compared, depending upon the Transient Period setting). See EVM (in %) .
This result is the difference in time of the PRACH data relative to the expected timing for the given subchannel setting (see Available Subchannels (Bit Mask) ). See 3GPP TS 25.211, 5.2.2 and 7.3 and 3GPP TS 25.214, 6.1.
 
Timing error is not available when 
Trigger Source
 is set to
 RF Rise
.
The measurement always measures the power in all 4096 chips of the PRACH preamble (regardless of the Transient Period setting), and also measures the power in up to 100 chips before and after the PRACH preamble (if there is a substantial amount of timing error, then fewer than 100 chips before or after the PRACH preamble will be measured and reported). The measurement reports the power in each chip relative to the greatest power measured in any of the chips.
This result is the EVM for each measured chip (either 3904 or 4096 chips, depending upon the Transient Period setting).
The rms EVM (see EVM (rms) (in %) ) and the peak EVM (see EVM (peak) (in %) ) for the entire PRACH preamble burst is also available.
A typical measurement result is shown below:
This measurement should be calibrated using the Calibrate Measurements function ( CALibration:MEASurements? ) when the temperature has changed by more than ± 10° C since the last calibration. If this situation exists, the integrity indicator value becomes 19 and a message is displayed indicating "Uncalibrated Due to Temperature".