Last updated: January 16, 2009
|
Performs a full preset of the test set. This is the remote equivalent of pressing the SHIFT Preset keys on the front panel of the test set. All parameters are set to their default values. All measurements are aborted the trigger arm is set to continuous. See Trigger Arm (Single or Continuous) Description . |
|
| Related Topics | See Full Preset for details about the *RST full preset. |
OUTPUT 714;"SYSTEM:PRESET2" !Full preset, trigger arm set to continuous. |
|
|
Performs a partial preset. This is the recommended command for users when a partial preset is needed during remote operation of the test set. Any call in process is disconnected and all measurements are aborted and inactivated. Measurement parameters are not changed. A partial preset will not modify any measurement settings including trigger arm. |
|
| Related Topics |
See Partial Preset for more details. |
OUTPUT 714;"SYSTEM:PRESET3" !Partial preset when in remote operation. |
|