Last updated: January 16, 2009
This section is only applicable to the lab application or a test application with the required feature license.
 
This example is for
 FDD Test Operating Mode
. The measurement is also available in
 Active Cell Operating Mode
.
This section provides an example of how to make HSDPA BLER measurements via remote program. The following program example assumes that the UE is connected to the RF IN/OUT connector.
The basic procedure to test HSDPA BLER is as follows:
 INITiate:HBLerror 
command to start the measurement.
 READ:HBLerror? 
command to both initiate and fetch the measurement as a sequential operation). 10 ! HSDPA Block Error Ratio Measurement Programming Example 20 ! 3GPP TS 34.121 6.3A Maximum Input Level for HS-PDSCH 30 ! Reception (16QAM) 40 ! 50 Testset=714 60 ! 70 !***Set up test parameters*** 80 ! 90 OUTPUT Testset;"CALL:OPERating:MODE FDDTest" 100 ! Set Operating Mode to FDD Test 110 OUTPUT Testset;"CALL:POWer -25.7" 120 ! Set Cell Power to -25.7 dB 130 OUTPUT Testset;"CALL:SERVice:RBTest:RAB HSDParmc12" 140 ! Set Channel Type to 12.2k RMC + HSDPA 150 OUTPUT Testset;"CALL:FDDTest:FRC:TYPE QAM1" 160 ! Set FRC Type to H-Set 1 16QAM 170 OUTPUT Testset;"CALL:FDDTest:MACHs:NTRans 1" 180 ! Set FDD Test Number of Tranmissions to 1 190 OUTPUT Testset;"CALL:FDDTest:MACHs:RVSequence `6'" 200 ! Set FDD Test RV Sequence to 6,0,0,0,0,0,0,0 210 OUTPUT Testset;"CALL:FDDTest:HRNTi `32'" 220 ! Set FDD Test Primary H-RNTI (Hex) as needed 230 OUTPUT Testset;"CALL:MS:POWer:TARGet 20" 240 ! Set UE Target Power to 20 or 18 dBm 250 OUTPUT Testset;"CALL:FDDTest:DPCHannel:HSDPa -13" 260 ! Set HSDPA FDD Test DPCH Level to -13 dB 270 OUTPUT Testset;"CALL:FDDTest:HSSCchannel -13" 280 ! Set FDD Test HS-SCCH 1 Level to -13 dB 290 ! 300 !***Set up measurement parameters*** 310 ! 320 OUTPUT Testset;"SETup:HBLerror:COUNt 500" 330 ! Set Number of blocks to test to 500 340 OUTPUT Testset;"SETup:HBLerror:CONTinuous OFF" 350 ! Set Trigger Arm to Single 360 ! 370 CLEAR SCREEN 380 PRINT "Configure the UE to synchronize to the test " 390 PRINT "set, demodulate the HS-SCCH and HS-PDSCH " 400 PRINT "channels and generate an HS-DPCCH." 410 PRINT 420 PRINT "Press CONTINUE" 430 PRINT 440 ! 450 PAUSE 460 ! 470 !***INITiate and FETCh measurements*** 480 ! 490 OUTPUT Testset;"INITiate:HBLerror" 500 ! Initiate an HBLER measurement 510 OUTPUT Testset;"FETCh:HBLerror?" 520 ENTER Testset;Int,Ratio,R,Ack,Nack,Sdtx,Num,Mcqi 530 ! 540 !***Print measurement results*** 550 ! 560 PRINT "HSDPA Block Error Ratio Results:" 570 PRINT 580 PRINT "Integrity Indicator = ",Int 590 PRINT "Block Error Ratio (%) = ",Ratio 600 PRINT "Information Bit Throughput (kbps) = ",R 610 PRINT "Positive Acknowledgments = ",Ack 620 PRINT "Negative Acknowledgments = ",Nack 630 PRINT "Statistical DTXs = ",Sdtx 640 PRINT "Number of Blocks Tested = ",Num 650 PRINT "Median Channel Quality Indicator = ",Mcqi 660 ! 670 END 680 !