Last updated: January 16, 2009
This section provides an example of how to make waveform quality measurements via GPIB. The following program example assumes that the mobile station's (UE's) antenna output is connected to the RF IN/OUT connector, and that the mobile station is synchronized to the test set and is transmitting an uplink signal.
The basic procedure to test waveform quality is as follows:
10 OUTPUT 714;"SETup:WWQuality:CONTinuous Off" !Set the waveform quality 20 !measurement to single trigger mode. 30 OUTPUT 714;"SETup:WWQuality:TIMeout 1S"!Set a timeout value of 1 second 40 !in case the measurement cannot be made. 50 OUTPUT 714;"SETup:WWQuality:COUNt 5" !Set multi-measurements to 5 and 60 !enable multi-measurements. 70 OUTPUT 714;"SETup:WWQuality:TSLot 11" !Set the measurement to 80 !measure waveform quality during timeslot 11. 90 OUTPUT 714;"INITiate:WWQuality" !Start the waveform quality measurement. 100 OUTPUT 714;"FETCh:WWQuality?" !Query the integrity indicator and all 110 !results for the waveform quality measurement. 120 ENTER 714;Integrity,Evm,Ferr,Ooff,Perr,Merr,Terr,Pcde !Enter the 130 !returned integrity indicator and measurement values into variables. 140 IF Integrity<>0 THEN !Check the integrity value. 150 PRINT "Measurement problem; check for signal level over/under range condition." 160 ELSE 170 ! Process measurement results 180 END IF 190 END
Integrity
 stores the returned integrity indicator value (see 
Integrity Indicator
); 0 means a successful measurement with no errors.
Evm
 returns the maximum error vector magnitude result.
Ferr
 returns the worst case frequency error result.
Ooff
 returns the maximum origin offset result.
Perr
 returns the maximum phase error result.
Merr
 returns the maximum magnitude error result.
Terr
 returns the worst case timing error in chips.
Pcde
 returns the maximum peak code domain error.