Last updated: January 16, 2009
HS-DPCCH
.
HS-DPCCH
.
HS-DPCCH Trigger Subslot Alignment
setting, you must first decrease the
HS-DPCCH Measurement Interval
setting appropriately.
Trigger Source
is set to
Immediate
or
External
.
Timing Error
results are not available when
Trigger Source
is set to
Immediate
.
AckNack
, a valid result is returned for Beta
hsacknak
, NaN is returned for Beta
hscqi
. Likewise, when
HS-DPCCH Trigger Slot Alignment
is set to
CQI1
or
CQI2
, a valid result is returned for Beta
hscqi
, NaN is returned for Beta
hsacknak
.
If
Over Range
(5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set.
If
(6) is returned, the measured signal is below the expected input level.
Under Range
If
Cannot Correlate
(17) is returned, the test set cannot demodulate the signal from the mobile station (UE). Make sure the uplink scrambling code from the mobile station matches the UL Scrambling setting on the test set (see
CALL:UPLink
).
If
Uncalibrated Due to Temperature
(19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. See
Calibrating the Test Set
.
See Integrity Indicator .