Last updated: January 16, 2009
 Manual
, ensure that 
Maximum Power Threshold for Test Manual
 is greater than 
Minimum Power Threshold for Test Manual
. Otherwise, the measurement will return a result of "fail", as you've specified that none of the measured timeslots be considered for pass/fail.
 
If
 Over Range
 (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set. 
 
If
 Under Range
 (6) is returned, the measured signal is below the expected input level.
 
If
 Uncalibrated Due to Temperature
 (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. 
Calibrating the Test Set
.
 
Unable to Cal; Power unstable 
(24) is returned if, during test segments E-H, the UE does not properly respond to power control during the re-range periods.
See Integrity Indicator .