This section is only applicable to the lab application.
Ping is a tool to help check system interconnects. The test set has a Ping feature that allows you to ping either the DUT IP Address or an alternate address specified by you (see How Do I Ping a Device From the Test Set? ). An IP datagram (technically an Internet Control Message Protocol (ICMP) Echo Request message) is sent from the test set to the ping target, and expects a response from the target. You can define the size of the IP datagram and the Internet Protocol to use (whether IPv4 or IPv6) when using this feature. The default packet size is 64 bytes for both IPv4 and IPv6. If a response is received it is recorded on the test set's display.
Ping is the simplest implementation of the Data Channel feature. If you are trying to debug a system that is not responding to a full network setup (for example a WAP setup), try pinging the DUT from a computer attached to the network. Experiment with very large packets, very long timeouts and continuous pings.
If the connection is good, then the device returns a packet to the test set and the packet transfer information is displayed on the test set's screen (see Ping Data Display ). The figure below shows the kind of information that is displayed on the Ping screen. In this example, the Ping Count has been set to ping 10 times. Note that on average it took 1248 ms to complete a ping.
LAN 2 PORT
 (see the Tip in 
LAN 2 PORT
for how to identify the support of LAN 2 PORT), both the 
LAN PORT
 and the 
LAN 2 PORT
 are required to be physically connected to the same subnet to ping a DUT. Undoubtedly the 
LAN IP Address
 and the 
LAN IP Address 2 (Data+)
 must also be set correctly.
LAN 2 PORT
, you only need to set the 
LAN IP Address
 correctly to ping a DUT from the test set, no physical connection to a subnet is required.
LAN 2 PORT
 due to hardware restriction and the 
Ping Protocol 
is set to 
IPv6
,then ping to a DUT (the 
Device to Ping 
is set to 
DUT
) will cause an error indicating that the requested operation is not supported.
Ping Protocol 
is set to 
IPv6
, the 
Ping6 Setup
 middle menu is displayed after 
Ping Setup
 (
F1
), and the Alternate Ping6 Address is divided into four parts to simplify the manual input: 
Alternate Ping6 Address Prefix, Upper (Hex)
, 
Alternate Ping6 Address Prefix, Lower (Hex)
, 
Alternate Ping6 Address IID, Upper (Hex)
, 
Alternate Ping6 Address IID, Lower (Hex)
.
Ping Protocol 
is set to 
IPv6
, the parameter of 
Ping Timeout 
is grayed out with a fixed value of 5 seconds.