This section is only applicable to the lab application.
|
This command enables or disables forwarding of subnet traffic to the DUT IP Address. See DUT Routing State for more information. |
|
OUTPUT 714;"CALL:MS:IP:ADDRess:ROUTing:STATe OFF" ! Turns off the DUT routing state. |
|
|
Sets/queries the DUT IPv6 Prefix . |
|
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers.
Double-colon "::" can be used in the IPv6 address as valid. Moreover, "::" can be suffixed at the end of the 19 characters which is also a valid IPv6 address prefix. For example: 2009:1:2:3 and 2009:1:2:3:: are all valid IPv6 address prefixes for the GPIB parameter setting. |
|
| Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. | |
| "" (Null) | |
|
Requirements |
|
OUTPUT 714;"CALL:MS:IP:ADDRess:IP6:PREFix '2009:1:2:3::'" !Sets the DUT IPv6 prefix to 2009:1:2:3::. |
|
|
Sets/queries the IPv4 address of the second primary PDP Context. |
|
| "" | |
|
Requirements |
|
OUTPUT 714;"CALL:MS:IP:ADDRess2 `130.29.179.219'" !Sets the address of second primay PDP Context to 130.29.179.219. |
|
| Sets/queries the type of the communication the test set will use when setting up a connection with the DUT, See DUT IP Version . | |
| IP4 | |
| Lab Application Revision: G.00.09 and above | |
OUTPUT 714;"CALL:MS:IP:VERSion IP4" ! Sets the DUT IP Version to IPv4. |
|
| Sets/queries the DUT IP 2 Version, the type of the communication the test set will use when setting up a connection with the DUT, See DUT IP 2 Version . | |
| IP4 | |
| Lab Application Revision: G.01.00 and above | |
OUTPUT 714;"CALL:MS:IP:VERSion 2 IP4" ! Sets the DUT IP 2 Version to IPv4. |
|