Last updated: January 16, 2009
This section is only applicable to the lab application.
|
Sets/queries the Routing Area Code (RAC) .
This parameter can only be set when
PS Domain Information
is set to |
|
| Same as setting. | |
| 1 | |
| Requirements | Test or Lab Application Revision: A.01 and above |
OUTPUT 714;"CALL:CELL:RACODE 2" ! Sets the routing area code to 2. |
|