:JOBS:ACQuire:COMPlete?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:ACQuire:COMPlete?
Query Response
{1 | 0}
Description
Queries the state of the measurement acquisition for a running FlexOTO Station. Always follow the :JOBS:ACQuire:COMPlete? query with an *OPC? query.
Use an *OPC? query to pause program execution while waiting for FlexOTO to complete waveform acquisition and analysis. Then, you can return measurement results.
:JOBS:ACQuire:COMPlete? query can only be sent to a FlexOTO Station. Sending this command to FlexOTO Hardware Diagram will result in an error.
Example Command Sequence
station.write(':TPRogram:SETup:MEASurements APOWer,PPHRatio')
station.write(':TPRogram:SETup:ADD')
jobids = station.query(':TPRogram:RUN?')
station.query(':JOBS:ACQuire:COMPlete?')
station.query('*OPC?')