:SYSTem:GTLocal
Flex Apps:
                                                FlexDCA
                                                FlexRT
                                                FlexPLL
                                                FlexOTO
                                            FlexOTO Instance:
                                                Hardware Diagram
                                                Stations
                                            Command Syntax
:SYSTem:GTLocal
Description
Places FlexOTO in local mode which allows operation via the front panel. This is useful if you need the user to perform a front-panel task. The next command that is sent to the instrument returns it to remote mode. When ending a program, you should always issue this command to return control to the front panel.
Requires FlexOTO revision A.07.00 and above.