SCPI Subsystems
FlexOTO Instance:
Hardware Diagram
The following picture shows the SCPI subsystems that are used to control features in FlexOTO Hardware Diagram (shown in blue) and FlexOTO Stations (shown in green). Some commands and subsystem control both FlexOTO Hardware Diagram and FlexOTO Stations. The FlexOTO Commands table lists all FlexOTO commands with their Hardware Diagram or Station support.
Use the:
:CALibratesubsystem to calibrate DCA-M modules.:CONFiguresubsystem to build the Hardware Diagram.:DISCsubsystem to save zip results files, Hardware Diagram and Station setup files, and screen images.:DISPlaysubsystem to configure FlexOTO's GUI (Graphical User Interface).:EUSagesubsystem to configure and query the Job Timing Diagram.:JOBSsubsystem to query Job Results.:STATussubsystem to set and query status registers.:SYSTemsubsystem to view and set basic system level settings.:TPRogramsubsystem to configure the Test Programs.:STARt, :STOP, and:RUNNingroot commands to start and end Station child processes.:ACQuire:COMPlete?command to determine when measurement acquisition has completed.