exit Command
FlexOTO Instance:
Hardware Diagram
This command instructs the instrument driver to disconnect from the instrument hardware and end the driver process. The command is sent from FlexOTO when the user clicks Exit in the Instrument Connection Setup dialog or the :INSTrument:DISConnect command is sent to FlexOTO. This command does not expect a return value.
exit command is sent to the Instrument Driver
Command Sent from FlexOTO
exit
Response Returned from Driver
This command does not provide a return value.