:DISPlay:CTHeme
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISPlay:CTHeme {"Tungsten" | "Aluminum"}
Query Syntax
:DISPlay:CTHeme?
Description
Selects one of two user-interface themes that affects the look of FlexPLL's window and dialogs. The placing of double or single quotes around the string argument is required. Tungsten is the Factory Preset theme. A Default Setup does not change the selected theme.
To invert the background color of the graph, use the :DISPlay:GRAPh:INVertcommand.
This command supports the DEFault common child command.